Part Number: TMDSIDK572
In the project example of MCSPI_Loopback_idkAM572x_c66xExampleProject, running result is failed, i.e. the data in receive buffer and data in transmit buffer is different.
AM572x idk board uses McSPI3 as Industries Inputs and this example uses McSPI3, but in the code of mcspiLoopbackApp.c \ padConfigprcmEnable(), configure SPI1 instead to configure SPI3.
void padConfig_prcmEnable()
{
#if defined (SOC_DRA72x) || (SOC_DRA75x) || defined (SOC_DRA78x)
Board_initCfg boardCfg;
boardCfg = BOARD_INIT_PINMUX_CONFIG |
BOARD_INIT_MODULE_CLOCK;
Board_init(boardCfg);
#endif
/* Loopback mode is not available for MCSPI. To test Loopback on McSPI,
* Receive Bit is enabled on both Tx and Rx pins of McSPI
*/
#if defined(SOC_AM571x) || defined (SOC_AM572x) || defined (SOC_AM574x)
HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_UART2_CTSN, 0x00050002);
HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_UART2_RTSN, 0x00010001);
HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_SPI1_SCLK,0x000C0000);
HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_SPI1_D1,0x000C0000);
HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_SPI1_D0,0x000C0000);
HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_SPI1_CS0,0x00060000);
#if defined (_TMS320C6X)
/*
* AM57x DSP does not have a default Xbar connection for UART
* interrupts, need to use a reserved IRQ Xbar instance for Xbar
* interrupt configuration
*/
/* Use reserved XBAR_INST_DSP1_IRQ_34 */
CSL_xbarIrqConfigure(CSL_XBAR_IRQ_CPU_ID_DSP1, CSL_XBAR_INST_DSP1_IRQ_34, CSL_XBAR_UART3_IRQ);
#endif
#if defined (SOC_AM572x) || defined(SOC_AM574x)
HW_WR_REG32(CSL_MPU_CORE_PAD_IO_REGISTERS_REGS+CSL_CONTROL_CORE_PAD_IO_PAD_SPI1_CS1,0x00060000);
#endif
#endif
#if defined (SOC_TDA2XX) || defined(SOC_TDA2PX) || defined (SOC_TDA2EX)
/*Pad configurations */
HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_UART1_RXD,0x00040000);
HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_UART1_TXD,0x00040000);
HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_SPI1_SCLK,0x000C0000);
HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_SPI1_D1,0x000C0000);
HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_SPI1_D0,0x000C0000);
HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_SPI1_CS0,0x00060000);
#if defined (SOC_TDA2XX) || defined(SOC_TDA2PX)
HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_SPI1_CS1,0x00060000);
#endif
/* IPU1 Crossbar */
CSL_xbarIrqConfigure(CSL_XBAR_IRQ_CPU_ID_IPU1, CSL_XBAR_INST_IPU1_IRQ_44, CSL_XBAR_UART1_IRQ);
#endif
#if defined(SOC_TDA3XX)
/*MCSPI1 prcm*/
HW_WR_REG32(SOC_L4PER_CM_CORE_BASE + CM_L4PER_MCSPI1_CLKCTRL, 0x02);
while (HW_RD_REG32(SOC_L4PER_CM_CORE_BASE + CM_L4PER_MCSPI1_CLKCTRL) !=
0x02U)
{
;
}
HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_UART1_RXD,0x00040000);
HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_UART1_TXD,0x00000000);
HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_SPI1_CS0,0x00040000);
HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_SPI1_SCLK,0x00040000);
HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_SPI1_D0,0x00040000);
HW_WR_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_SPI1_D1,0x00040000);
/* IPU1 crossbar */
#if defined (__TI_ARM_V7M4__)
CSL_xbarIrqConfigure(CSL_XBAR_IRQ_CPU_ID_IPU1, CSL_XBAR_INST_IPU1_IRQ_44, CSL_XBAR_UART1_IRQ);
#elif defined(_TMS320C6X)
CSL_xbarIrqConfigure(CSL_XBAR_IRQ_CPU_ID_DSP1, CSL_XBAR_INST_DSP1_IRQ_44, CSL_XBAR_UART1_IRQ);
#endif
#endif
#if defined(SOC_AM335x) || defined(SOC_AM437x)
uint32_t ctrlModBase;
/* UART */
ctrlModBase = CHIPDBBaseAddress(CHIPDB_MOD_ID_CONTROL_MODULE, UART_INSTANCE);
HW_WR_REG32(ctrlModBase+PIN_UART0_TXD, PIN_MODE(0));
HW_WR_REG32(ctrlModBase+PIN_UART0_RXD, PIN_MODE(0) | PIN_RX_ACTIVE);
/* SPI0 */
ctrlModBase = CHIPDBBaseAddress(CHIPDB_MOD_ID_CONTROL_MODULE, MCSPI_INSTANCE);
HW_WR_REG32(ctrlModBase+PIN_SPI0_SCLK, PIN_MODE(0) | PIN_RX_ACTIVE);
HW_WR_REG32(ctrlModBase+PIN_SPI0_D0, PIN_MODE(0) | PIN_RX_ACTIVE);
HW_WR_REG32(ctrlModBase+PIN_SPI0_D1, PIN_MODE(0) | PIN_RX_ACTIVE);
HW_WR_REG32(ctrlModBase+PIN_SPI0_CS0, PIN_MODE(0) | PIN_RX_ACTIVE);
#endif
}