Part Number: TDA4VMXEVM
Dear experts,
I want to test UB940 Deserializer, its output is MIPI CSI-2.
Can I connect its output directly to the CSI-2 EXP at the bottom of EVM without using Fusion Expansion board ?
Thanks,
Brahim
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VMXEVM
Dear experts,
I want to test UB940 Deserializer, its output is MIPI CSI-2.
Can I connect its output directly to the CSI-2 EXP at the bottom of EVM without using Fusion Expansion board ?
Thanks,
Brahim
Hello Brahim,
Well, if it supports MIPI output connector, you could connect. But we have not really tested this deserializer with CSIRx, so there could be surprises.
Rgds,
Brijesh