Other Parts Discussed in Thread: OMAP-L138, OMAP-L137, OMAPL138
Hi All,
We have a both a OMAP-L138 LogicPD EVM board and a OMAP-L137 Spectrum DigitalEVM board. We will be eventually building a custom board with one or the other. In the meantime I've created ARM code that so far runs on both...
I do need to be able to determine which OMAP I have to further setup peripheral devices and resources. So looking for the easiest way I can determine the OMAP type at runtime -- if this is possible...
Thanks for your time & effort!
Steve Speier