This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: GP evm/RTOS/USB3.0

Part Number: AM5728
Other Parts Discussed in Thread: TUSB8041

I am using AM5728 GP evm board.
I am using RTOS and the version is processor_sdk_rtos_am57xx_5_02_00_10.

I want to use USB3.0 on GP evm board.
I have checked the examples provided by the RTOS SDK.
And I found that the 'USB_HostMsc_idkAM572x_armExampleProject' example supports USB3.0 on the idk board.

Can I test USB3.0 by modifying the source code of the example on the GP evm board?
I saw that this is not possible with GP evm board. However, does the TUSB8041 chip on the GP evm board support USB3.0?

I wonder whether it is impossible because of the hardware design of the GP evm board, or because there is no content in the source code of the example.

If there is a way to test USB3.0 on GP evm board, I would appreciate it.
Finally, i plan to use USB3.0 in device mode.

I would appreciate your reply.

Thank you.