Other Parts Discussed in Thread: AM5718, DRA722, PMP
Hi TI Team,
I am using TMDXIDK5718, REV 1.3B and ti-processor-sdk-linux-rt-am57xx-evm-06.02.00.81-Linux-x86-Install.
This is working fine and i can see complete log on tera term.
My Question: I am trying to disable UART3(ttyS2) as console and want to use this for my different serial application.
(1) I have made following changes in /board-support/u-boot-2019.01+gitAUTOINC+a141f7abfd-ga141f7abfd/arch/arm/dts/am57xx-idk-common.dtsi.Compiled u-Boot, Copied new MLO and u-boot.img in SD card.
chosen {
stdout-path = &uart1;
};
&uart1 {
status = "okay";
interrupts-extended = <&crossbar_mpu GIC_SPI 67 IRQ_TYPE_LEVEL_HIGH
&dra7_pmx_core 0x3E0>;
};
(2) I have made following changes in /board-support/linux-rt-4.19.79+gitAUTOINC+5baf382c8f-g5baf382c8f/arch/arm/boot/dts/am57xx-idk-common.dtsi. I Compiled am571x-idk.dts to am571x-idk.dtb file and copied in /rootfs/boot of the SD card.
chosen {
stdout-path = &uart1;
};
&uart1 {
status = "okay";
interrupts-extended = <&crossbar_mpu GIC_SPI 67 IRQ_TYPE_LEVEL_HIGH
&dra7_pmx_core 0x3E0>;
};
&uart3 {
status = "okay";
};
After inserting SD card in Board, following messages appear on tera term. Please help me for what i am missing to disable UART3 as a console.
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.19.79-rt28-g5baf382c8f (student@ubuntu) (gcc version 8.3.0 (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36))) #2 SMP PREEMPT RT Mon May 11 17:38:05 IST 2020
[ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
[ 0.000000] CPU: div instructions available: patching division code
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[ 0.000000] OF: fdt: Machine model: TI AM5718 IDK
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000095800000, size 56 MiB
[ 0.000000] OF: reserved mem: initialized node ipu2-memory@95800000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 64 MiB
[ 0.000000] OF: reserved mem: initialized node dsp1-memory@99000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x000000009d000000, size 32 MiB
[ 0.000000] OF: reserved mem: initialized node ipu1-memory@9d000000, compatible id shared-dma-pool
[ 0.000000] cma: Reserved 24 MiB at 0x00000000be400000
[ 0.000000] OMAP4: Map 0x00000000bfd00000 to (ptrval) for dram barrier
[ 0.000000] DRA722 ES2.0
[ 0.000000] random: get_random_bytes called from start_kernel+0xb0/0x488 with crng_init=0
[ 0.000000] percpu: Embedded 15 pages/cpu s32224 r8192 d21024 u61440
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 202048
[ 0.000000] Kernel command line: console=ttyS2,115200n8 root=PARTUUID=fe7d99b9-02 rw rootfstype=ext4 rootwait
[ 0.000000] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 641360K/815104K available (10240K kernel code, 343K rwdata, 2748K rodata, 2048K init, 277K bss, 26288K reserved, 147456K cma-reserved, 234496K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0x(ptrval) - 0x(ptrval) (12256 kB)
[ 0.000000] .init : 0x(ptrval) - 0x(ptrval) (2048 kB)
[ 0.000000] .data : 0x(ptrval) - 0x(ptrval) ( 344 kB)
[ 0.000000] .bss : 0x(ptrval) - 0x(ptrval) ( 278 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=2 to nr_cpu_ids=1.
[ 0.000000] rcu: RCU priority boosting: priority 1 delay 500 ms.
[ 0.000000] No expedited grace period (rcu_normal_after_boot).
[ 0.000000] Tasks RCU enabled.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] GIC: Using split EOI/Deactivate mode
[ 0.000000] OMAP clockevent source: timer1 at 32786 Hz
[ 0.000000] arch_timer: cp15 timer(s) running at 6.14MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
[ 0.000005] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
[ 0.000011] Switching to timer-based delay loop, resolution 162ns
[ 0.000292] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[ 0.000296] OMAP clocksource: 32k_counter at 32768 Hz
[ 0.000781] Console: colour dummy device 80x30
[ 0.000914] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
[ 0.000922] pid_max: default: 32768 minimum: 301
[ 0.001061] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001070] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001744] CPU: Testing write buffer coherency: ok
[ 0.001777] CPU0: Spectre v2: using ICIALLU workaround
[ 0.002024] /cpus/cpu@0 missing clock-frequency property
[ 0.002055] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.059919] Setting up static identity map for 0x80200000 - 0x80200060
[ 0.099922] rcu: Hierarchical SRCU implementation.
[ 0.160392] EFI services will not be available.
[ 0.180053] smp: Bringing up secondary CPUs ...
[ 0.180066] smp: Brought up 1 node, 1 CPU
[ 0.180077] SMP: Total of 1 processors activated (12.29 BogoMIPS).
[ 0.180087] CPU: All CPU(s) started in HYP mode.
[ 0.180095] CPU: Virtualization extensions available.
[ 0.180723] devtmpfs: initialized
[ 0.220260] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[ 0.220637] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.220660] futex hash table entries: 256 (order: 2, 16384 bytes)
[ 0.223357] pinctrl core: initialized pinctrl subsystem
[ 0.224276] DMI not present or invalid.
[ 0.224756] NET: Registered protocol family 16
[ 0.227481] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.228394] omap_hwmod: l3_main_2 using broken dt data from ocp
[ 0.433925] OMAP GPIO hardware version 0.1
[ 0.466407] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[ 0.466423] hw-breakpoint: maximum watchpoint size is 8 bytes.
[ 0.468432] OMAP DMA hardware revision 0.0
[ 0.514653] edma 43300000.edma: memcpy is disabled
[ 0.520886] edma 43300000.edma: TI EDMA DMA engine driver
[ 0.534056] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver (LinkedList1/2/3 supported)
[ 0.540415] omap-iommu 40d01000.mmu: 40d01000.mmu registered
[ 0.540968] omap-iommu 40d02000.mmu: 40d02000.mmu registered
[ 0.541567] omap-iommu 58882000.mmu: 58882000.mmu registered
[ 0.542167] omap-iommu 55082000.mmu: 55082000.mmu registered
[ 0.542828] iommu: Adding device 58820000.ipu to group 1
[ 0.543049] iommu: Adding device 55020000.ipu to group 2
[ 0.543432] iommu: Adding device 40800000.dsp to group 0
[ 0.545091] SCSI subsystem initialized
[ 0.546739] palmas 0-0058: Irq flag is 0x00000004
[ 0.574147] palmas 0-0058: Muxing GPIO 2f, PWM 0, LED 0
[ 0.576070] SMPS12: supplied by regulator-dummy
[ 0.578080] SMPS3: supplied by VMAIN
[ 0.579937] SMPS45: supplied by regulator-dummy
[ 0.582117] SMPS6: supplied by VMAIN
[ 0.584113] SMPS7: supplied by VMAIN
[ 0.586252] SMPS8: supplied by VMAIN
[ 0.587797] SMPS9: supplied by VMAIN
[ 0.588165] random: fast init done
[ 0.589053] LDO1: supplied by VMAIN
[ 0.591698] LDO2: supplied by VMAIN
[ 0.601555] LDO3: supplied by VMAIN
[ 0.611572] LDO4: supplied by VMAIN
[ 0.621623] LDO5: supplied by regulator-dummy
[ 0.622604] LDO6: supplied by regulator-dummy
[ 0.623563] LDO7: supplied by regulator-dummy
[ 0.624520] LDO8: supplied by regulator-dummy
[ 0.625454] LDO9: supplied by VMAIN
[ 0.631959] LDOLN: supplied by VMAIN
[ 0.641630] LDOUSB: supplied by VMAIN
[ 0.655711] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
[ 0.656016] media: Linux media interface: v0.10
[ 0.656074] videodev: Linux video capture interface: v2.00
[ 0.656201] pps_core: LinuxPPS API ver. 1 registered
[ 0.656212] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.656239] PTP clock support registered
[ 0.656279] EDAC MC: Ver: 3.0.0
[ 0.661844] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
[ 0.662125] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
[ 0.671185] Advanced Linux Sound Architecture Driver Initialized.
[ 0.672485] clocksource: Switched to clocksource arch_sys_counter
[ 0.686459] NET: Registered protocol family 2
[ 0.687384] tcp_listen_portaddr_hash hash table entries: 512 (order: 2, 16384 bytes)
[ 0.687426] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.687513] TCP bind hash table entries: 8192 (order: 5, 229376 bytes)
[ 0.687768] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.687907] UDP hash table entries: 512 (order: 3, 32768 bytes)
[ 0.687964] UDP-Lite hash table entries: 512 (order: 3, 32768 bytes)
[ 0.688242] NET: Registered protocol family 1
[ 0.718968] RPC: Registered named UNIX socket transport module.
[ 0.718983] RPC: Registered udp transport module.
[ 0.718992] RPC: Registered tcp transport module.
[ 0.719001] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.720786] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
[ 0.722667] Initialise system trusted keyrings
[ 0.722890] workingset: timestamp_bits=14 max_order=18 bucket_order=4
[ 0.732974] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.743823] NFS: Registering the id_resolver key type
[ 0.743862] Key type id_resolver registered
[ 0.743874] Key type id_legacy registered
[ 0.743949] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.746868] Key type asymmetric registered
[ 0.746884] Asymmetric key parser 'x509' registered
[ 0.747056] bounce: pool size: 64 pages
[ 0.747104] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[ 0.747119] io scheduler noop registered
[ 0.747130] io scheduler deadline registered
[ 0.747413] io scheduler cfq registered (default)
[ 0.747427] io scheduler mq-deadline registered
[ 0.747438] io scheduler kyber registered
[ 0.756120] pinctrl-single 4a003400.pinmux: 282 pins, size 1128
[ 0.756387] pinctrl-single 4a002e8c.pinmux: please update dts to use #pinctrl-cells = <1>
[ 0.756458] pinctrl-single 4a002e8c.pinmux: initialized with no interrupts
[ 0.756470] pinctrl-single 4a002e8c.pinmux: 1 pins, size 4
[ 0.783169] dra7-pcie 51000000.pcie: Linked as a consumer to phy-4a094000.pciephy.1
[ 0.783553] dra7-pcie 51000000.pcie: WA for Errata i870 not applied
[ 0.783721] dra7-pcie 51000000.pcie: host bridge /ocp/axi@0/pcie@51000000 ranges:
[ 0.783764] dra7-pcie 51000000.pcie: IO 0x20003000..0x20012fff -> 0x00000000
[ 0.783795] dra7-pcie 51000000.pcie: MEM 0x20013000..0x2fffffff -> 0x20013000
[ 1.784085] dra7-pcie 51000000.pcie: Phy link never came up
[ 1.784299] dra7-pcie 51000000.pcie: PCI host bridge to bus 0000:00
[ 1.784319] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 1.784332] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
[ 1.784344] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
[ 1.790669] PCI: bus0: Fast back to back transfers disabled
[ 1.796578] PCI: bus1: Fast back to back transfers enabled
[ 1.796636] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff 64bit]
[ 1.796657] pci 0000:00:00.0: PCI bridge to [bus 01-ff]
[ 1.797366] pcieport 0000:00:00.0: Signaling PME with IRQ 170
[ 1.797711] pcieport 0000:00:00.0: AER enabled with IRQ 170
[ 1.805123] V3_3D: supplied by smps9
[ 1.805462] vtt_fixed: supplied by V3_3D
[ 1.883675] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 1.889853] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 45, base_baud = 3000000) is a 8250
[ 1.891756] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 46, base_baud = 3000000) is a 8250
[ 2.933057] console [ttyS2] enabled
[ 2.939758] omap_rng 48090000.rng: Random Number Generator ver. 20
[ 2.947258] random: crng init done
[ 2.951267] omapdss_dss 58000000.dss: Linked as a consumer to regulator.20
[ 2.958345] DSS: OMAP DSS rev 6.1
[ 2.966193] omapdss_hdmi5 58040000.encoder: Linked as a consumer to regulator.13
[ 2.973826] omapdss_hdmi5 58040000.encoder: Dropping the link to regulator.13
[ 3.003363] brd: module loaded
[ 3.019455] loop: module loaded
[ 3.032050] m25p80 spi0.0: s25fl256s1 (32768 Kbytes)
[ 3.037114] 7 fixed-partitions partitions found on MTD device spi0.0
[ 3.043499] Creating 7 MTD partitions on "spi0.0":
[ 3.048316] 0x000000000000-0x000000040000 : "QSPI.SPL"
[ 3.054776] 0x000000040000-0x000000140000 : "QSPI.u-boot"
[ 3.061432] 0x000000140000-0x0000001c0000 : "QSPI.u-boot-spl-os"
[ 3.068660] 0x0000001c0000-0x0000001d0000 : "QSPI.u-boot-env"
[ 3.075631] 0x0000001d0000-0x0000001e0000 : "QSPI.u-boot-env.backup1"
[ 3.083331] 0x0000001e0000-0x0000009e0000 : "QSPI.kernel"
[ 3.089988] 0x0000009e0000-0x000002000000 : "QSPI.file-system"
[ 3.098064] libphy: Fixed MDIO Bus: probed
[ 3.162520] davinci_mdio 48485000.mdio: davinci mdio revision 1.6, bus freq 1000000
[ 3.170217] davinci_mdio 48485000.mdio: detected phy mask fffffffc
[ 3.181361] libphy: 48485000.mdio: probed
[ 3.185399] davinci_mdio 48485000.mdio: phy[0]: device 48485000.mdio:00, driver Micrel KSZ9031 Gigabit PHY
[ 3.195100] davinci_mdio 48485000.mdio: phy[1]: device 48485000.mdio:01, driver Micrel KSZ9031 Gigabit PHY
[ 3.206170] cpsw 48484000.ethernet: Detected MACID = 44:ea:d8:17:b5:4e
[ 3.212818] cpsw 48484000.ethernet: initialized cpsw ale version 1.4
[ 3.219203] cpsw 48484000.ethernet: ALE Table size 1024
[ 3.224503] cpsw 48484000.ethernet: cpts: overflow check period 500 (jiffies)
[ 3.233167] cpsw 48484000.ethernet: cpsw: Detected MACID = 44:ea:d8:17:b5:4f
[ 3.242726] i2c /dev entries driver
[ 3.253501] sdhci: Secure Digital Host Controller Interface driver
[ 3.259713] sdhci: Copyright(c) Pierre Ossman
[ 3.265650] sdhci-pltfm: SDHCI platform and OF driver helper
[ 3.272918] omap_gpio 4805d000.gpio: Could not set line 27 debounce to 200000 microseconds (-22)
[ 3.281745] sdhci-omap 4809c000.mmc: Got CD GPIO
[ 3.286912] sdhci-omap 4809c000.mmc: Linked as a consumer to regulator.26
[ 3.294104] sdhci-omap 4809c000.mmc: Linked as a consumer to regulator.11
[ 3.301116] sdhci-omap 4809c000.mmc: Dropping the link to regulator.11
[ 3.307840] sdhci-omap 4809c000.mmc: Linked as a consumer to regulator.2
[ 3.314911] sdhci-omap 4809c000.mmc: Linked as a consumer to regulator.11
[ 3.321875] sdhci-omap 4809c000.mmc: no pinctrl state for ddr_3_3v mode
[ 3.355609] mmc0: SDHCI controller on 4809c000.mmc [4809c000.mmc] using ADMA
[ 3.363762] sdhci-omap 480b4000.mmc: Linked as a consumer to regulator.2
[ 3.370747] sdhci-omap 480b4000.mmc: Dropping the link to regulator.2
[ 3.377401] sdhci-omap 480b4000.mmc: Linked as a consumer to regulator.2
[ 3.410405] mmc1: SDHCI controller on 480b4000.mmc [480b4000.mmc] using ADMA
[ 3.430010] NET: Registered protocol family 10
[ 3.433746] mmc0: host does not support reading read-only switch, assuming write-enable
[ 3.436695] mmc0: new high speed SDHC card at address aaaa
[ 3.453284] mmcblk0: mmc0:aaaa JULIE 29.7 GiB
[ 3.460413] Segment Routing with IPv6
[ 3.464214] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 3.471241] NET: Registered protocol family 17
[ 3.474002] mmcblk0: p1 p2
[ 3.480584] Key type dns_resolver registered
[ 3.485082] Registering SWP/SWPB emulation handler
[ 3.489925] omap_voltage_late_init: Voltage driver support not added
[ 3.496422] Power Management for TI OMAP4+ devices.
[ 3.501364] ti-iodelay 4844a000.padconf: Set reg 0x18c Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[ 3.510287] ti-iodelay 4844a000.padconf: Set reg 0x1a4 Delay(a: 119 g: 0), Elements(C=0 F=3)0x29003
[ 3.513597] Loading compiled-in X.509 certificates
[ 3.544157] ti-iodelay 4844a000.padconf: Set reg 0x1b0 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[ 3.562988] ti-iodelay 4844a000.padconf: Set reg 0x1bc Delay(a: 18 g: 0), Elements(C=0 F=0)0x29000
[ 3.571997] ti-iodelay 4844a000.padconf: Set reg 0x1c8 Delay(a: 894 g: 0), Elements(C=1 F=12)0x2902c
[ 3.591099] ti-iodelay 4844a000.padconf: Set reg 0x1d4 Delay(a: 30 g: 0), Elements(C=0 F=0)0x29000
[ 3.610058] ti-iodelay 4844a000.padconf: Set reg 0x1e0 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[ 3.628919] ti-iodelay 4844a000.padconf: Set reg 0x1ec Delay(a: 23 g: 0), Elements(C=0 F=0)0x29000
[ 3.647873] ti-iodelay 4844a000.padconf: Set reg 0x1f8 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[ 3.656560] dmm 4e000000.dmm: workaround for errata i878 in use
[ 3.666825] ti-iodelay 4844a000.padconf: Set reg 0x360 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[ 3.675748] ti-iodelay 4844a000.padconf: Set reg 0x194 Delay(a: 152 g: 0), Elements(C=0 F=4)0x29004
[ 3.684862] ti-iodelay 4844a000.padconf: Set reg 0x1ac Delay(a: 206 g: 0), Elements(C=0 F=6)0x29006
[ 3.693957] ti-iodelay 4844a000.padconf: Set reg 0x1b8 Delay(a: 78 g: 0), Elements(C=0 F=2)0x29002
[ 3.702967] ti-iodelay 4844a000.padconf: Set reg 0x1c4 Delay(a: 2 g: 0), Elements(C=0 F=0)0x29000
[ 3.711886] ti-iodelay 4844a000.padconf: Set reg 0x1d0 Delay(a: 266 g: 0), Elements(C=0 F=7)0x29007
[ 3.720981] ti-iodelay 4844a000.padconf: Set reg 0x1dc Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[ 3.729916] ti-iodelay 4844a000.padconf: Set reg 0x1e8 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[ 3.735101] dmm 4e000000.dmm: initialized all PAT entries
[ 3.746747] ti-iodelay 4844a000.padconf: Set reg 0x1f4 Delay(a: 43 g: 0), Elements(C=0 F=1)0x29001
[ 3.755756] ti-iodelay 4844a000.padconf: Set reg 0x200 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[ 3.764676] ti-iodelay 4844a000.padconf: Set reg 0x368 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[ 3.773596] ti-iodelay 4844a000.padconf: Set reg 0x190 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[ 3.782517] ti-iodelay 4844a000.padconf: Set reg 0x1a8 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[ 3.791435] ti-iodelay 4844a000.padconf: Set reg 0x1b4 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[ 3.800354] ti-iodelay 4844a000.padconf: Set reg 0x1c0 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[ 3.809274] ti-iodelay 4844a000.padconf: Set reg 0x1d8 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[ 3.818194] ti-iodelay 4844a000.padconf: Set reg 0x1e4 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[ 3.827114] ti-iodelay 4844a000.padconf: Set reg 0x1f0 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[ 3.836034] ti-iodelay 4844a000.padconf: Set reg 0x1fc Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[ 3.844954] ti-iodelay 4844a000.padconf: Set reg 0x364 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
[ 3.856291] omapdss_hdmi5 58040000.encoder: Linked as a consumer to regulator.13
[ 3.864034] omapdss_hdmi5 58040000.encoder: Dropping the link to regulator.13
[ 3.873622] omapdss_hdmi5 58040000.encoder: Linked as a consumer to regulator.13
[ 3.881591] omapdss_dss 58000000.dss: bound 58001000.dispc (ops dispc_component_ops)
[ 3.889937] omapdss_dss 58000000.dss: bound 58040000.encoder (ops hdmi5_component_ops)
[ 3.899461] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 3.906190] mmc1: new DDR MMC card at address 0001
[ 3.911320] [drm] No driver support for vblank timestamp query.
[ 3.917300] [drm] Cannot find any crtc or sizes
[ 3.923742] [drm] Initialized omapdrm 1.0.0 20110917 for omapdrm.0 on minor 0
[ 3.931810] hctosys: unable to open rtc device (rtc0)
[ 3.933262] mmcblk1: mmc1:0001 R1J56L 13.8 GiB
[ 3.933986] mmcblk1boot0: mmc1:0001 R1J56L partition 1 4.00 MiB
[ 3.934709] mmcblk1boot1: mmc1:0001 R1J56L partition 2 4.00 MiB
[ 3.942597] mmcblk1rpmb: mmc1:0001 R1J56L partition 3 128 KiB, chardev (244:0)
[ 3.968907] ALSA device list:
[ 3.971891] No soundcards found.
[ 4.791386] EXT4-fs (mmcblk0p2): recovery complete
[ 4.802823] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 4.811019] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 4.828170] devtmpfs: mounted
[ 4.834225] Freeing unused kernel memory: 2048K
[ 4.838921] Run /sbin/init as init process
[ 4.962780] [drm] Cannot find any crtc or sizes
[ 5.166936] systemd[1]: System time before build time, advancing clock.
[ 5.204637] systemd[1]: systemd 239 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
[ 5.226687] systemd[1]: Detected architecture arm.
Welcome to Arago 2019.11!
[ 5.275631] systemd[1]: Set hostname to <am57xx-evm>.
[ 5.603478] systemd[1]: File /lib/systemd/system/systemd-journald.service:36 configures an IP firewall (IPAddressDeny=any), but the local system does not support BPF/cgroup based firewalling.
[ 5.620623] systemd[1]: Proceeding WITHOUT firewalling in effect! (This warning is only shown for the first loaded unit using IP firewalling.)
[ 5.936869] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ 6.002196] systemd[1]: Listening on Process Core Dump Socket.
[ OK ] Listening on Process Core Dump Socket.
[ 6.044857] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 6.083415] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 6.113058] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password Requests to Wall Directory Watch.
[ OK ] Listening on Network Service Netlink Socket.
[ OK ] Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Reached target Slices.
[ OK ] Created slice system-getty.slice.
[ OK ] Reached target Swap.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ OK ] Reached target Paths.
[ OK ] Reached target Remote File Systems.
[ OK ] Listening on Journal Socket.
Mounting POSIX Message Queue File System...
Starting Create list of required st…ce nodes for the current kernel...
Starting Remount Root and Kernel File Systems...
[ OK ] Listening on udev Kernel Socket.
[ 6.610395] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
Starting udev Coldplug all Devices...
Mounting Temporary Directory (/tmp)...
Mounting Kernel Debug File System...
Starting Load Kernel Modules...
[ OK ] Started Hardware RNG Entropy Gatherer Daemon.
[ 6.857859] cmemk: loading out-of-tree module taints kernel.
[ OK ] [ 6.877717] CMEMK module: reference Linux version 4.19.79
Listening on Journal Socket (/dev/log).
[ 6.897715] cmemk initialized
Starting Journal Service...
[ 6.941017] cryptodev: driver 1.9 loaded.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Started Create list of required sta…vice nodes for the current kernel.
[ OK ] Started Remount Root and Kernel File Systems.
[ OK ] Mounted Temporary Directory (/tmp).
[ OK [ 7.156084] usbcore: registered new interface driver usbfs
] Mounted Kernel Debug File System.
[ 7.173814] usbcore: registered new interface driver hub
[ 7.206003] usbcore: registered new device driver usb
Starting Create Static Device Nodes in /dev...
[ 7.257523] usbcore: registered new interface driver ftdi_sio
[ 7.282777] usbserial: USB Serial support registered for FTDI USB Serial Device
[ OK ] Started Load Kernel Modules.
[ OK ] Started Create Static Device Nodes in /dev.
Starting udev Kernel Device Manager...
[ OK ] Reached target Local File Systems (Pre).
Mounting /media/ram...
[ OK ] Reached target Containers.
Mounting /var/volatile...
Starting Apply Kernel Variables...
Mounting Kernel Configuration File System...
[ OK ] Started udev Kernel Device Manager.
[ OK ] Started Journal Service.
[ OK ] Mounted /media/ram.
[ OK ] Mounted /var/volatile.
[ OK ] Started Apply Kernel Variables.
[ OK ] Mounted Kernel Configuration File System.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Flush Journal to Persistent Storage...
[ OK ] Started Load/Save Random Seed.
[ 8.447645] systemd-journald[130]: Received request to flush runtime journal from PID 1
[ OK ] Started Flush Journal to Persistent Storage.
Starting Create Volatile Files and Directories...
[ OK ] Started Create Volatile Files and Directories.
Starting Update UTMP about System Boot/Shutdown...
Starting Network Time Synchronization...
Starting Network Service...
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ OK ] Started Network Service.
Starting Wait for Network to be Configured...
Starting Network Name Resolution...
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Time Synchronized.
[ OK ] Started Network Name Resolution.
[ OK ] Reached target Network.
[ OK ] Reached target Host and Network Name Lookups.
[ 10.090242] omap-rproc 58820000.ipu: ignoring dependency for device, assuming no driver
[ 10.147897] omap-rproc 58820000.ipu: ignoring dependency for device, assuming no driver
[ 10.273161] omap-rproc 58820000.ipu: assigned reserved memory node ipu1-memory@9d000000
[ 10.281357] remoteproc remoteproc0: 58820000.ipu is available
[ 10.502728] omap-rproc 55020000.ipu: ignoring dependency for device, assuming no driver
[ 10.569378] omap-rproc 55020000.ipu: ignoring dependency for device, assuming no driver
[ 10.714445] omap-rproc 55020000.ipu: assigned reserved memory node ipu2-memory@95800000
[ 10.800108] remoteproc remoteproc1: 55020000.ipu is available
[ 10.841504] remoteproc remoteproc0: powering up 58820000.ipu
[ 10.847210] remoteproc remoteproc0: Booting fw image dra7-ipu1-fw.xem4, size 6884184
[ 10.892916] omap-rproc 40800000.dsp: ignoring dependency for device, assuming no driver
[ 10.893143] omap-rproc 40800000.dsp: ignoring dependency for device, assuming no driver
[ 10.893152] omap-rproc 40800000.dsp: assigned reserved memory node dsp1-memory@99000000
[ 10.893295] remoteproc remoteproc2: 40800000.dsp is available
[ 11.050504] remoteproc remoteproc1: powering up 55020000.ipu
[ 11.050525] remoteproc remoteproc1: Booting fw image dra7-ipu2-fw.xem4, size 3747220
[ 11.050622] omap-iommu 55082000.mmu: 55082000.mmu: version 2.1
[ 11.529288] Driver for 1-wire Dallas network protocol.
[ 11.593170] omap-des 480a5000.des: OMAP DES hw accel rev: 2.2
[ 11.622564] omap-des 480a5000.des: will run requests pump with realtime priority
[ 11.776871] omap_hdq 480b2000.1w: OMAP HDQ Hardware Rev 0.:. Driver in Interrupt mode
[ 11.812890] ov2659 0-0030: Sensor detection failed (3030, 0)
[ 11.989184] w1_master_driver w1_bus_master1: Attaching one wire slave 01.000000000000 crc 3d
[ 12.050035] omap_gpio 4805b000.gpio: Could not set line 7 debounce to 20000 microseconds (-22)
[ 12.068630] w1_master_driver w1_bus_master1: Family 1 for 01.000000000000.3d is not registered.
[ 12.088125] palmas-rtc 48070000.i2c:tps659038@58:tps659038_rtc: rtc core: registered 48070000.i2c:tps659038@58:tps659038_rtc as rtc0
[ 12.088257] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 12.088472] remoteproc remoteproc1: registered virtio0 (type 7)
[ 12.088747] remoteproc remoteproc1: remote processor 55020000.ipu is now up
[ 12.546219] omap_rtc 48838000.rtc: registered as rtc1
[ 12.743121] net eth0: initializing cpsw version 1.15 (0)
[ 12.773229] vpe 489d0000.vpe: loading firmware vpdma-1b8.bin
[ 12.883335] Micrel KSZ9031 Gigabit PHY 48485000.mdio:00: attached PHY driver [Micrel KSZ9031 Gigabit PHY] (mii_bus:phy_addr=48485000.mdio:00, irq=POLL)
[ 12.901398] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 12.983200] vip 48970000.vip: loading firmware vpdma-1b8.bin
[ 13.042972] net eth1: initializing cpsw version 1.15 (0)
[ 13.165593] Micrel KSZ9031 Gigabit PHY 48485000.mdio:01: attached PHY driver [Micrel KSZ9031 Gigabit PHY] (mii_bus:phy_addr=48485000.mdio:01, irq=POLL)
[ 13.169649] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
[ 13.535804] phy phy-4a084000.phy.3: Linked as a consumer to regulator.21
[ 13.539067] phy phy-4a085000.phy.4: Linked as a consumer to regulator.21
[ OK ] Found device /dev/ttyS2.
[ OK ] Started udev Coldplug all Devices.
[ 13.881749] ahci 4a140000.sata: controller can't do 64bit DMA, forcing 32bit
[ 13.899081] virtio_rpmsg_bus virtio1: rpmsg host is online
[ 13.899173] remoteproc remoteproc0: registered virtio1 (type 7)
[ 13.899183] remoteproc remoteproc0: remote processor 58820000.ipu is now up
[ 13.937093] CAN device driver interface
[ 13.937793] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 13.974233] omap-sham 4b101000.sham: hw accel on OMAP rev 4.3
[ 14.027059] c_can_platform 4ae3c000.can: c_can_platform device registered (regs=c1ddb8f3, irq=90)
[ 14.196319] virtio_rpmsg_bus virtio0: creating channel rpmsg-rpc addr 0x65
[ 14.196540] virtio_rpmsg_bus virtio0: creating channel rpmsg-rpc addr 0x66
[ 14.225179] omap-aes 4b500000.aes: OMAP AES hw accel rev: 3.3
[ 14.242670] vip 48970000.vip: VPDMA firmware loaded
[ 14.243056] vpe 489d0000.vpe: Device registered as /dev/video0
[ 14.243136] omap-aes 4b500000.aes: will run requests pump with realtime priority
[ 14.288810] omap-aes 4b700000.aes: OMAP AES hw accel rev: 3.3
[ 14.304090] omap-aes 4b700000.aes: will run requests pump with realtime priority
[ 15.249258] remoteproc remoteproc2: powering up 40800000.dsp
[ 15.249279] remoteproc remoteproc2: Booting fw image dra7-dsp1-fw.xe66, size 20482260
[ 15.256230] omap-iommu 40d01000.mmu: 40d01000.mmu: version 3.0
[ 15.256270] omap-iommu 40d02000.mmu: 40d02000.mmu: version 3.0
[ 15.537719] virtio_rpmsg_bus virtio2: rpmsg host is online
[ 15.537806] remoteproc remoteproc2: registered virtio2 (type 7)
[ 15.537814] remoteproc remoteproc2: remote processor 40800000.dsp is now up
[ 15.767139] [drm] Initialized pvr 1.17.4948957 20110701 for 56000000.gpu on minor 1
[ 15.812856] virtio_rpmsg_bus virtio2: creating channel rpmsg-proto addr 0x3d
[ 15.942977] omap-hdmi-audio omap-hdmi-audio.0.auto: snd-soc-dummy-dai <-> 58040000.encoder mapping ok
[ 15.942991] omap-hdmi-audio omap-hdmi-audio.0.auto: ASoC: no DMI vendor name!
[ 16.212456] ahci 4a140000.sata: forcing port_map 0x0 -> 0x1
[ 16.302611] davinci_mdio 4b232400.mdio: davinci mdio revision 1.6, bus freq 1000000
[ 16.302622] libphy: 4b232400.mdio: probed
[ 16.347620] davinci_mdio 4b232400.mdio: phy[0]: device 4b232400.mdio:00, driver TI TLK10X 10/100 Mbps PHY
[ 16.347629] davinci_mdio 4b232400.mdio: phy[1]: device 4b232400.mdio:01, driver TI TLK10X 10/100 Mbps PHY
[ 16.442659] davinci_mdio 4b2b2400.mdio: davinci mdio revision 1.6, bus freq 1000000
[ 16.442671] libphy: 4b2b2400.mdio: probed
[ 16.469443] davinci_mdio 4b2b2400.mdio: phy[0]: device 4b2b2400.mdio:00, driver TI TLK10X 10/100 Mbps PHY
[ 16.469452] davinci_mdio 4b2b2400.mdio: phy[1]: device 4b2b2400.mdio:01, driver TI TLK10X 10/100 Mbps PHY
[ 16.480856] remoteproc remoteproc3: 4b234000.pru is available
[ 16.481014] pru-rproc 4b234000.pru: PRU rproc node pru@4b234000 probed successfully
[ 16.484053] remoteproc remoteproc4: 4b238000.pru is available
[ 16.484202] pru-rproc 4b238000.pru: PRU rproc node pru@4b238000 probed successfully
[ 16.484615] remoteproc remoteproc5: 4b2b4000.pru is available
[ 16.484766] pru-rproc 4b2b4000.pru: PRU rproc node pru@4b2b4000 probed successfully
[ 16.485149] remoteproc remoteproc6: 4b2b8000.pru is available
[ 16.485305] pru-rproc 4b2b8000.pru: PRU rproc node pru@4b2b8000 probed successfully
[ 16.577285] cpsw 48484000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off
[ 16.577332] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 16.764011] prueth pruss1_eth: pruss_fw_drop_untagged_vlan 0
[ 16.764022] prueth pruss1_eth: pruss MC Mask (Port 0) ff:ff:ff:ff:ff:ff
[ 16.764031] prueth pruss1_eth: pruss MC Mask (Port 1) ff:ff:ff:ff:ff:ff
[ 16.770207] prueth pruss1_eth: TI PRU ethernet (type 0) driver initialized
[ 17.069849] prueth pruss2_eth: pruss_fw_drop_untagged_vlan 0
[ 17.069862] prueth pruss2_eth: pruss MC Mask (Port 0) ff:ff:ff:ff:ff:ff
[ 17.069870] prueth pruss2_eth: pruss MC Mask (Port 1) ff:ff:ff:ff:ff:ff
[ 17.079263] prueth pruss2_eth: TI PRU ethernet (type 0) driver initialized
[ 18.478041] ahci 4a140000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
[ 18.586634] ahci 4a140000.sata: flags: ncq sntf pm led clo only pmp pio slum part ccc apst
[ 18.744946] scsi host0: ahci
[ 18.748538] ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a1410ff] port 0x100 irq 82
[ 19.145065] ata1: SATA link down (SStatus 0 SControl 300)
[** ] A start job is running for Wait for… to be Configured (14s / no limit)[ 20.708441] dwc3 48890000.usb: Failed to get clk 'ref': -2
[ 20.771123] dwc3 488d0000.usb: Failed to get clk 'ref': -2
[ 20.874816] rpmsg_rpc virtio0.rpmsg-rpc.-1.101: probing service dce-callback with src 1024 dst 101
[ 20.981435] rpmsg_rpc virtio0.rpmsg-rpc.-1.101: published functions = 4
[ 21.001420] rpmsg_rpc virtio0.rpmsg-rpc.-1.102: probing service rpmsg-dce with src 1025 dst 102
[ 21.121896] rpmsg_rpc virtio0.rpmsg-rpc.-1.102: published functions = 9
[ 21.293934] NET: Registered protocol family 45
[*** ] A start job is running for Wait for… to be Configured (15s / no limit)[ 21.845793] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 21.851339] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 1
[ 22.019958] xhci-hcd xhci-hcd.1.auto: hcc params 0x0220f04c hci version 0x100 quirks 0x0000000002010010
[ 22.130554] xhci-hcd xhci-hcd.1.auto: irq 179, io mem 0x48890000
[ 22.134291] pruss_intc_irq_set_affinity: event 21 not configured: ch = -1, host = -1
[ 22.134416] pruss_intc_irq_set_affinity: event 23 not configured: ch = -1, host = -1
[ 22.134511] pruss_intc_irq_set_affinity: event 27 not configured: ch = -1, host = -1
[ 22.156022] iep ptp bc clkid -1
[ 22.156078] remoteproc remoteproc4: powering up 4b238000.pru
[ 22.160372] remoteproc remoteproc4: Booting fw image ti-pruss/am57xx-pru1-prueth-fw.elf, size 7152
[ 22.160734] pruss 4b200000.pruss: configured system_events[63-0] = 00600000,08a00000
[ 22.160743] pruss 4b200000.pruss: configured intr_channels = 0x0000032a host_intr = 0x000002aa
[ 22.160752] remoteproc remoteproc4: remote processor 4b238000.pru is now up
[ 22.160802] net eth3: started
[ 22.161642] IPv6: ADDRCONF(NETDEV_UP): eth3: link is not ready
[ 22.250888] pruss_intc_irq_set_affinity: event 20 not configured: ch = -1, host = -1
[ 22.251017] pruss_intc_irq_set_affinity: event 22 not configured: ch = -1, host = -1
[ 22.251106] pruss_intc_irq_set_affinity: event 26 not configured: ch = -1, host = -1
[ 22.251241] remoteproc remoteproc3: powering up 4b234000.pru
[ 22.253208] remoteproc remoteproc3: Booting fw image ti-pruss/am57xx-pru0-prueth-fw.elf, size 7124
[ 22.253571] pruss 4b200000.pruss: configured system_events[63-0] = 00000600,04500000
[ 22.253580] pruss 4b200000.pruss: configured intr_channels = 0x000000d5 host_intr = 0x00000155
[ 22.253589] remoteproc remoteproc3: remote processor 4b234000.pru is now up
[ 22.253636] net eth2: started
[ 22.253848] IPv6: ADDRCONF(NETDEV_UP): eth2: link is not ready
[ 22.291354] pruss_intc_irq_set_affinity: event 21 not configured: ch = -1, host = -1
[ 22.291480] pruss_intc_irq_set_affinity: event 23 not configured: ch = -1, host = -1
[ 22.291569] pruss_intc_irq_set_affinity: event 27 not configured: ch = -1, host = -1
[ 22.305542] iep ptp bc clkid -1
[ 22.305596] remoteproc remoteproc6: powering up 4b2b8000.pru
[ 22.305701] remoteproc remoteproc6: Booting fw image ti-pruss/am57xx-pru1-prueth-fw.elf, size 7152
[ 22.306079] pruss 4b280000.pruss: configured system_events[63-0] = 00600000,08a00000
[ 22.306088] pruss 4b280000.pruss: configured intr_channels = 0x0000032a host_intr = 0x000002aa
[ 22.306096] remoteproc remoteproc6: remote processor 4b2b8000.pru is now up
[ 22.306154] net eth5: started
[ 22.307084] IPv6: ADDRCONF(NETDEV_UP): eth5: link is not ready
[ 22.345433] pruss_intc_irq_set_affinity: event 20 not configured: ch = -1, host = -1
[ 22.345558] pruss_intc_irq_set_affinity: event 22 not configured: ch = -1, host = -1
[ 22.345653] pruss_intc_irq_set_affinity: event 26 not configured: ch = -1, host = -1
[ 22.345784] remoteproc remoteproc5: powering up 4b2b4000.pru
[ 22.345890] remoteproc remoteproc5: Booting fw image ti-pruss/am57xx-pru0-prueth-fw.elf, size 7124
[ 22.346309] pruss 4b280000.pruss: configured system_events[63-0] = 00000600,04500000
[ 22.346318] pruss 4b280000.pruss: configured intr_channels = 0x000000d5 host_intr = 0x00000155
[ 22.346328] remoteproc remoteproc5: remote processor 4b2b4000.pru is now up
[ 22.346372] net eth4: started
[ 22.354764] IPv6: ADDRCONF(NETDEV_UP): eth4: link is not ready
[ *** ] A start job is running f[ 22.782332] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 4.19
or Wait for… to be Configured (16s / no limit)[ 22.795718] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 22.807664] usb usb1: Product: xHCI Host Controller
[ 22.813187] usb usb1: Manufacturer: Linux 4.19.79-rt28-g5baf382c8f xhci-hcd
[ 22.820186] usb usb1: SerialNumber: xhci-hcd.1.auto
[ 22.833105] hub 1-0:1.0: USB hub found
[ 22.841491] hub 1-0:1.0: 1 port detected
[ 22.852456] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 22.866900] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 2
[ 22.879854] xhci-hcd xhci-hcd.1.auto: Host supports USB 3.0 SuperSpeed
[ 22.897069] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 22.916382] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 4.19
[ 22.929938] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 22.944636] usb usb2: Product: xHCI Host Controller
[ 22.954866] usb usb2: Manufacturer: Linux 4.19.79-rt28-g5baf382c8f xhci-hcd
[ 22.971527] usb usb2: SerialNumber: xhci-hcd.1.auto
[ 22.983764] hub 2-0:1.0: USB hub found
[ 22.992184] hub 2-0:1.0: 1 port detected
[ OK ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
[ OK ] Created slice system-systemd\x2dfsck.slice.
Starting File System Check on /dev/mmcblk0p1...
[ OK ] Reached target System Initialization.
Starting Reboot and dump vmcore via kexec...
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on dropbear.socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
[ OK ] Started Periodic Command Scheduler.
[ OK ] Started Redis In-Memory Data Store.
Starting Login Service...
Starting Lightning Fast Webserver With Light System Requirements...
Starting rc.pvr.service...
Starting TI IPC Daemon...
Starting /etc/rc.local Compatibility...
Starting Permit User Sessions...
[ 31.921730] PVR_K: UM DDK-(4948957) and KM DDK-(4948957) match. [ OK ]
Starting Print notice about GPLv3 packages...
Starting Simple Network Management Protocol (SNMP) Daemon....
Starting Enable and configure wl18xx bluetooth stack...
Starting Save/Restore Sound Card State...
Starting Avahi mDNS/DNS-SD Stack...
[ OK ] Started D-Bus System Message Bus.
[ OK ] Started Job spooling tools.
[ OK ] Started Daily rotation of log files.
[ OK ] Reached target Timers.
Starting RPC Bind Service...
Starting TI MultiCore Tools Daemon...
[ OK ] Started File System Check on /dev/mmcblk0p1.
[ OK ] Started Reboot and dump vmcore via kexec.
[ OK ] Started Lightning Fast Webserver With Light System Requirements.
[ OK ] Started rc.pvr.service.
[ OK ] Started TI IPC Daemon.
[ OK ] Started Permit User Sessions.
[ OK ] Started Enable and configure wl18xx bluetooth stack.
[ OK ] Started Save/Restore Sound Card State.
[ OK ] Started RPC Bind Service.
[ OK ] Started TI MultiCore Tools Daemon.
[ OK ] Started NFS status monitor for NFSv2/3 locking..
[ OK ] Reached target Sound Card.
Starting weston.service...
Mounting /run/media/mmcblk0p1...
[ OK ] Started Login Service.
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Mounted /run/media/mmcblk0p1.
[ OK ] Started Simple Network Management Protocol (SNMP) Daemon..
[ OK ] Started /etc/rc.local Compatibility.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyS2.
[ OK ] Reached target Login Prompts.
Starting Synchronize System and HW clocks...
[ OK ] Started Synchronize System and HW clocks.
[ OK ] Started weston.service.
Starting Matrix GUI...
Starting telnetd.service...
[ OK ] Started Matrix GUI.
[ OK ] Started telnetd.service.
Starting thttpd.service...
[ OK ] Started thttpd.service.
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPLv3 packages:
autoconf
bash-dev
bash
bc
binutils-dev
binutils
bison-dev
bison
cifs-utils
cpio
cpp-symlinks
cpp
dosfstools
elfutils-dev
elfutils
findutils
g++-symlinks
g++
gawk
gcc-symlinks
gcc
gdb
gdbc6x
gdbserver
gettext
glmark2
gstreamer1.0-libav
gzip
hidapi
libasm1
libbfd
libcairo-perf-utils
libdw1
libelf1
libgdbm-compat4
libgdbm-dev
libgdbm6
libgettextlib
libgettextsrc
libgmp10
libidn2-0
libmavconn
libmpc3
libmpfr6
libreadline-dev
libreadline7
libunistring2
m4-dev
m4
make
mavlink
mavros-extras
mavros-msgs
mavros
nettle
parted
pdm-anomaly-detection
socketcan-interface
swig-dev
swig
which
If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
[ OK ] Started Print notice about GPLv3 packages.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org am57xx-evm ttyS2
Arago 2019.11 am57xx-evm ttyS2
am57xx-evm login: root
root@am57xx-evm:~# dmesg | grep ttyS*
[ 0.000000] Kernel command line: console=ttyS2,115200n8 root=PARTUUID=fe7d99b9-02 rw rootfstype=ext4 rootwait
[ 1.889853] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 45, base_baud = 3000000) is a 8250
[ 1.891756] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 46, base_baud = 3000000) is a 8250
[ 2.933057] console [ttyS2] enabled
[ 5.936869] systemd[1]: Created slice system-serial\x2dgetty.slice.
root@am57xx-evm:~#