Part Number: TDA4VM
Hi,
I have four questions about ethfw.
1. Is /lib/firmware/the app_remoteswitchcfg_server_pdk_mem_map_strip.xer5f which I find in TI prebuild folder the ethfw ?
2. If the Ethfw is placed under this directory(/lib/firmware/), will TI have a mechanism to bring him up by default ? Or what config do we need to open to start Ethfw.
3. Which COM port will receive the message that ethfw R5F output. My environment is from TI's prebuild image (PSDK_6.2.0).
Linux kernel messages output messages from COM port 6, but there are no messages output from COM port 7 ~ 9.
If there is no message, does it mean that ethfw on our platform may not start normally.
4. The following are our files in rootfs, is it enough?
lib/firmware$ls -lh
total 51M
-rwxrwxr-x 1 allenhsu allenhsu 1.4M Jan 31 02:52 app_remoteswitchcfg_server_pdk_mem_map_strip.xer5f
drwxrwxr-x 2 allenhsu allenhsu 4.0K Jan 27 20:22 cadence
-rwxrwxr-x 1 allenhsu allenhsu 897K Jan 27 22:46 iwlwifi-3160-17.ucode
-rwxrwxr-x 1 allenhsu allenhsu 1.7M Jan 27 22:46 iwlwifi-8000C-13.ucode
-rwxrwxr-x 1 allenhsu allenhsu 2.3M Jan 27 22:46 iwlwifi-8000C-16.ucode
-rwxrwxr-x 1 allenhsu allenhsu 2.3M Jan 27 22:46 iwlwifi-8000C-21.ucode
-rwxrwxr-x 1 allenhsu allenhsu 2.1M Jan 27 22:46 iwlwifi-8000C-22.ucode
-rwxrwxr-x 1 allenhsu allenhsu 2.2M Jan 27 22:46 iwlwifi-8000C-27.ucode
-rwxrwxr-x 1 allenhsu allenhsu 2.3M Jan 27 22:46 iwlwifi-8000C-31.ucode
-rwxrwxr-x 1 allenhsu allenhsu 2.4M Jan 27 22:46 iwlwifi-8000C-34.ucode
-rwxrwxr-x 1 allenhsu allenhsu 2.4M Jan 27 22:46 iwlwifi-8000C-36.ucode
-rwxrwxr-x 1 allenhsu allenhsu 2.3M Jan 27 22:46 iwlwifi-8265-21.ucode
-rwxrwxr-x 1 allenhsu allenhsu 1.8M Jan 27 22:46 iwlwifi-8265-22.ucode
-rwxrwxr-x 1 allenhsu allenhsu 2.2M Jan 27 22:46 iwlwifi-8265-27.ucode
-rwxrwxr-x 1 allenhsu allenhsu 2.3M Jan 27 22:46 iwlwifi-8265-31.ucode
-rwxrwxr-x 1 allenhsu allenhsu 2.4M Jan 27 22:46 iwlwifi-8265-34.ucode
-rwxrwxr-x 1 allenhsu allenhsu 2.4M Jan 27 22:46 iwlwifi-8265-36.ucode
-rw-rw-r-- 1 allenhsu allenhsu 1.4M Feb 17 13:27 j7-c66_0-fw
-rw-rw-r-- 1 allenhsu allenhsu 1.4M Feb 17 13:27 j7-c66_1-fw
-rw-rw-r-- 1 allenhsu allenhsu 6.7M Feb 17 13:27 j7-c71_0-fw
-rw-rw-r-- 1 allenhsu allenhsu 126K Feb 17 13:27 j7-main-r5f0_0-fw
-rw-rw-r-- 1 allenhsu allenhsu 3.7M Feb 17 13:27 j7-main-r5f0_1-fw
-rwxrwxr-x 1 allenhsu allenhsu 107K Feb 7 22:40 jailhouse.bin
-rwxrwxr-x 1 allenhsu allenhsu 2.0K Jan 27 22:46 LICENCE.iwlwifi_firmware
drwxrwxr-x 2 allenhsu allenhsu 4.0K Feb 7 22:42 pru
-rwxrwxr-x 1 allenhsu allenhsu 242K Jan 27 22:45 pvdec_full_bin.fw
-rwxrwxr-x 1 allenhsu allenhsu 4.1K Jan 27 22:46 regulatory.db
-rwxrwxr-x 1 allenhsu allenhsu 1.2K Jan 27 22:46 regulatory.db.p7s
-rwxrwxr-x 1 allenhsu allenhsu 1.4M Feb 7 17:59 rgx.fw.22.104.208.318
-rwxrwxr-x 1 allenhsu allenhsu 1.4M Feb 7 17:59 rgx.fw.22.104.208.318.vz
drwxrwxr-x 2 allenhsu allenhsu 4.0K Jan 27 22:46 ti-connectivity
-rwxrwxr-x 1 allenhsu allenhsu 2.1M Jan 27 22:45 ti-display-sharing-j721e.bin