I am in the process of configuring the AM3517 SOM-M2 to run in a very low power sleep mode. So far the lowest I have been able to go is 20mA. My goal is to achieve a 1mA or lower sleep current draw. The supplier, LogicPD, has confirmed that this is possible, but it may require building the power state from the ground up. However, I have been unable to find information on configuring the power states in the TI processors wiki. Where would be a good place to start in adjusting the power states? What Kernel files would need to be modified? I would greatly appreciate any instructions you can provide, resources you can link me to, or other general suggestions towards achieving my goal.
Background: My pad configuration is minimal: 5V to MAIN_BATT_IN, ground lines, UARTs 1-3, and ethernet. VDDSHV is at 3.3V. Current is measured globally from my variable voltage supply, with all external ICs removed and ethernet disconnected. I am using the Linux PSP to configure the Kernel and u-boot. The Kernel is configured with power management and debugging, with USB, graphics, multimedia, and sound disabled. The only u-boot modification is the ETK lines have been muxed to GPIO.