What is the logic state of the SPI_TX line when inactive, between SPI transactions? We are using a resistor to pull the line to a known state, but would like to make it match the inactive state of the TX line so that we're not burning power over the resistor while the port is inactive (which is the majority of the time due to it's low duty cycle).
Thanks - AM