This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C5502 WDTOUT pulse width



Hi,

on our custom board we have connected the WDTOUT signal to a host microprocessor for detection of DSP failure. However, as far as I can tell the output pulse can only be stretched to a maximum of 4 clock cycles. If this is driven from the fast peripherals clocks which is configured at 150MHz then the output signal will only pulse for ~260ns. Is there any way to make this pulse wider? I guess one option would be to slow the fast peripherals clock, but that's not ideal.

Any other suggestions or is there something I've missed?

Chris

  • Hi,

     

    You can widen WDTOUT signal to set Timer CLK Register (CLK) CLKDIV register.

    Regards,

    Hyun

  • I didn't think I could.

    From Timers reference guide section 5.2 - Timer Clock Speed Register (CLK):

    The timer clock speed register (CLK) can be read to identify the internal clock
    frequency divider ratio for the timer. On the C5501/5502 device, the ratio is 1/1,
    meaning the internal timer clock (if used) is equal to the fast peripherals clock
    (SYSCLK1). Therefore, the CLKDIV field of CLK is always read as 0 on the
    C5501/5502 device.

    Chris