This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP-L138: when running helloworld example, it can't ping

Genius 13655 points

Part Number: OMAP-L138
Other Parts Discussed in Thread: SYSBIOS

Hello,

HW: OMAP-L138+DP83848 PHY

SW: NDK 2-25-01-11, nsp1-10-03-15

Configuring static IP address in syscfg and running helloworld example on C674x dsp core, it can print out 100M, ip and  mac address, but it existed after creating deamonnew, the code stopped in tidle.c or Hwi.c, winapp shows timesout. It can't ping. 

Thanks.
Rgds
Shine