Part Number: AM5728
Other Parts Discussed in Thread: SYSBIOS
Hi
I am using ti-processor-sdk-linux-am57xx-evm-04.03.00.05,which include opencl-1.1.14.10-r0.0 and opencv/3.1+gitAUTOINC+9b88e8c746-r3
I have read the TI OpenCV wiki, and I get the similar data:
when opencl off, for 1080P JPEG picture, Canny cost 145ms; when opencl on, Canny cost 17ms.
When I process two same pictures consecutively in the same program, the timing becomes strange
opencl on: Fisrt process: 11ms, Second process: 0.58ms; I try more image process, others always 0.5+ms
Q1:Why is there such a strange phenomenon?
I use OE to create a filesytem, which include dra7-dsp1-fw.xe66.opencl-monitor and dra7-dsp2-fw.xe66.opencl-monitor, which is work fine at openc on status.The above data is based on these two firmware tests
When I use the file system that comes with the SDK package, which dsp monitor firmware is work fine at opencl off, but opencl on, dsp will crash.
Q2: Why the SDK dsp monitor firmware will crash when opencl on? Can you recurrent it?
If you have any idea, please let me know.
Thanks.