This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3354: Cannot access Ethernet ports

Part Number: AM3354

Hi,

I am using AM3354 Processor  and facing the problem in detecting eth0 and eth1 (Not getting the ping response from customized AM3354 Processor board) in boot sequence the log is

[ 12.756896] remoteproc remoteproc0: powering up wkup_m3
[ 12.955206] wm8974 0-001a: Failed to issue reset
[ 12.960077] wm8974 0-001a: ASoC: failed to probe component -121
[ 13.067983] c_can_platform 481d0000.can can0: setting BTR=0209 BRPE=0000
[ 13.114837] davinci_phycore sound_iface: ASoC: failed to instantiate card -121
[ 13.137945] IPv6: ADDRCONF(NETDEV_CHANGE): can0: link becomes ready
[ 13.221101] davinci_phycore sound_iface: snd_soc_register_card failed (-121)
[ 13.273375] remoteproc remoteproc0: Booting fw image am335x-pm-firmware.elf, size 224296
[ 13.348930] davinci_phycore: probe of sound_iface failed with error -121
[ 13.383370] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x192
[ 13.390718] remoteproc remoteproc0: remote processor wkup_m3 is now up
[ 14.028238] net eth0: initializing cpsw version 1.12 (0)
[ 14.033918] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4
[ 14.040613] cpsw 4a100000.ethernet: ALE Table size 1024
[ 14.048641] net eth0: phy "/ocp/ethernet@4a100000/mdio@4a101000/ethernet-phy@0" not found on slave 0
[ 14.350347] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 14.691662] net eth1: initializing cpsw version 1.12 (0)
[ 14.699860] net eth1: phy "/ocp/ethernet@4a100000/mdio@4a101000/ethernet-phy@2" not found on slave 1
[ 14.940415] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
[ 16.037242] [drm] Initialized pvr 1.14.3699939 20110701 for 56000000.sgx on minor 1
[ OK ] Started Login Service.
[ 16.211674] PVR_K: UM DDK-(3699939) and KM DDK-(3699939) match. [ OK ]
[ OK ] Started rc.pvr.service.
Starting Autostart Qt 5 Demo...
[ OK ] Started Autostart Qt 5 Demo.
[ OK ] Reached target Multi-User System.


Bootloader : BareBox,

Kernel Version:4.14.78-bsp-yocto-am335x-pd19.1.1