This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Interrupt Controller initialization, unable to read registers

Other Parts Discussed in Thread: SYSCONFIG

Hi community

I am having a problem with the interrupt controller, looks like i forgot to route a required clock to the interrupt controller module.
At the moment i try to read the registers with the debugger, it tells me "Memory map prevented reading of target memory.."

Isn't it enough to enable the ICLK for the interrupt module? In the Technical Reference Manual, i can see that MPU_INTC_FCLK exists, but there is no PRCM register to enable the MPU_INTC_FCLK.

My code looks like this:

#define OMAP_PRCM_CORE_CM_REGS_PA  0x48004A00
#define OMAP_INTC_MPU_REGS_PA              0x48200000

#define CM_CLKEN_ICR         (1 << 29)
#define CM_IDLEST_ST_ICR   (1 << 29)

// ------------ interrupt controller (INTCPS) module initialization -----------
// softreset interrupt controller module
volatile OMAP_INTCPS_REGS* pIntrCtrlReg = (OMAP_INTCPS_REGS*)OMAP_INTC_MPU_REGS_PA;
pIntrCtrlReg->INTCPS_SYSCONFIG |= INTCPS_SYSCONFIG_SOFTRESET;
while ((pIntrCtrlReg->INTCPS_SYSSTATUS & INTCPS_SYSSTATUS_RESETDONE) == 0) {
    ;
}

// enable clock
volatile OMAP_PRCM_CORE_CM_REGS* pPrcmCoreRegs = (OMAP_PRCM_CORE_CM_REGS*)OMAP_PRCM_CORE_CM_REGS_PA;
pPrcmCoreRegs->CM_ICLKEN1_CORE |= CM_CLKEN_ICR;
while (pPrcmCoreRegs->CM_IDLEST1_CORE & CM_IDLEST_ST_ICR) {
    ;
}

 I have attached a screenshot of the debugger: