Part Number: XEVMK2LX
Other Parts Discussed in Thread: TCI6630K2L
Tool/software: Code Composer Studio
Hi,
I need to get rx and tx interrupts from UART1, I try:
#define UART_HWI_NUM 6
...
Hwi_Params_init(&hwiparams);
hwiparams.eventId = 233; // 234, 235
hwiparams.maskSetting = ti_sysbios_interfaces_IHwi_MaskingOption_ALL;
Error_init(&eb);
hwi = Hwi_create(UART_HWI_NUM, (Hwi_FuncPtr)&Uart_irq_handler, &hwiparams, &eb);
if (!hwi) {
return -1;
}
Hwi_enable();
Hwi_enableInterrupt(UART_HWI_NUM);
A 233-235 is a numbers from Table 7-24. CIC0 Event Inputs — C66x CorePac Secondary Interrupts at page 103 of tci6630k2l datasheet (SPRS893E.pdf). I see ipend = 0 flag in iir register of uart, that means interrupt is pending (according to Table 3-5 at page33 of UART periferal datasheet SPRUGP1.pdf), but my IRQ handler not called. What is wrong?