This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DDR PHY Control Register Read Latency (RL) Value



According to the TMS320C674x Memory Controller Guide: Read Latency = CAS latency + round-trip board delay- 1. (Units are clock cycles.)

 

The minimum clock cycle period supported (150MHz) is 6.7ns.  If propagation delay is 180ps/in, the traces would need to be 18 inches long to result in one clock cycle delay.  What value should I use for round-trip board delay if my traces are just under one inch long?

Also is CAS latency a specification of the memory chips.  For example, my memory chip's CAS#-to-CAS# delay t[CCD] is 2 clock cycles.  Is that the same thing as CAS latency?

  • Charles,

    I recommend using RL = CAS Latency + 1.  If the interface has timing issues, you can increase or decrease the number as necessary.

    CAS latency and CAS#-to-CAS# are not the same.  You should be able to find "CAS Latency" or "CL" in the DDR datasheet as in the attached example.

    -Tommy

  • Tommy,

    Thank you very much. 

    Your suggestion of RL  = CAS Latency + 1 results in a greater value than the user guide's recommendation.  It that because it's okay for this value to be too large but not too small, so a larger number gives you some headroom for unexpected tolerances? 

    Thanks,

    CJ

  • Charles,

    Yes, the +1 gives the memory interface more slack time so the DDR will still function ok.  I'm sure that RL = CL will also work for you, but I'd rather err on the side of caution at first and then speed things up later.

    -Tommy