Part Number: TMS320C6745
Hi
i have tried direct boot through NOR flash interface.
when doing so i got two EMA_CS2/ signals with address changing from 00,01,10&11 twice for EMA_BA0 & EMA_BA1. during this time EMA_A12 toEMA_A0 was "0000".
after the two EMA_cs2/ signal along with EMA_oe/ for reading a word twice the EMA_BA0 & EMA_BA1 was "11" and EMA_A12 toEMA_ A0 "0000".
there was no further signals in the EMIFA interface. what could be the reason? how can i proceed with instruction execution in direct boot mode?