Other Parts Discussed in Thread: DM3730
I'm using a DM3730 with multiple cameras. I have 4 cameras connected to the parallel interface (CPI). The cameras provide RGB output, 320x240 at approx 180fps, so I'm using CCDC->PREV->memory->RESZ as the ISP chain. The cameras provide HS, VS, and PCLK. I select between the cameras by tri-stating all but one off the bus. This works well, except when I'm switching cameras. Since the cameras aren't perfectly in sync with each other, switching causes the HS/VS/PCLK signals to not be exactly right. When I switch quickly, as when trying to get a single frame from each camera in a round robin fashion, the number of PRV_DONE interrupts I see is sometimes much, much less than the number of HS_VS interrupts. For example, I may see 190 HS_VS interrupts / second, 180 VD0 interrupts/second but only 10 PRV_DONE interrupts / second. My current theory is that the nonstandard HS/VS timing is confusing the Previewer. Can anyone provide more details about the Previewer and what conditions trigger a Previewer start or restart?