This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6678: PCIe switch for two End Points

Part Number: TMS320C6678
Other Parts Discussed in Thread: DS100MB203, TMS320C6657

Hi,

We want to use the following PCIe сsheme:

Where 1 - EVMC6678 board is as Root Complex; 2 - Switch DS100MB203 from Texas Instruments; 3, 4 - two identical End Points (these are our custom boards with tms320c6657 dsp).

The evmc6678 board manages switch 2 in order to communicates with boards 3 and 4.

We can successfully link the root complex and both endpoints in turn by link training. We need real time commuications. We want switch link from one endpoint to another in approx 50 microseconds, but the link training lasts more than several milliseconds.

Is there any way to avoid the link training or significantly reduce its time duration after switching from one end point to other? Can we do the link training only once or we must do it every time after switching?

Thank you.