Our customer wants to use a hardware error injection for PCIe between C6657 and other devices. Because their system under development must comply with IEC 61784-3, the system needs to implement the fault injection test function for PCIe that is related field communication.
What hardware error injection feature does the C6657 support for PCIe?
For example, the following features can be found in the PCIe User Guide.
- INV_ECRC and INV_LCRC in DIAG_CTRL register
- ACK_DISABLE in LANE_SKEW register
Is there any information for PCIe error injection?
Best regards,
Daisuke