Hello,
I'm using CCS version 4.2.0.10018 and SYS/BIOS 6.30.2.42 to develop an application for the TMS320DM6437. This processor is on a custom board that we have developed.
I need Ethernet support so I downloaded NDK 2.20.03.24. I have a few questions.
How and where do I "install" the NDK so that it is properly integrated with CCS and SYS/BIOS? This is no NDK setup file.
Is this a complete installation or is it a patch only? In other words, do I need to download a base version like NDK 2.20, and then patch it?
Do I also need the Network Support Package (NSP)?
Is NDK an extension of SYS/BIOS or XDCtools?
Do I configure it in CCS using XGCONF?
Thanks for your help. I searched but did not find answers to these questions.
Tim M