Other Parts Discussed in Thread: SYSBIOS
hi Sir
We are working on REL_210_V_H264_E_HP_DM365_02_00_00_11 project. It is a ccs3 project for h.264 project without System/bios,
Howerver we are trying to insert system/bios into this project , we got some problems and questions as below: (Please also link to here : Re: sdk / codec for ccs-only development for dm365)
1.We have trasformed REL_210_V_H264_E_HP_DM365_02_00_00_11 as a ccs4 project and it could be built properly and could be excuted by ccs4 environment properly.
However ,when we try to insert a SYS/BIOS moudule (RTSC configure file: .cfg file)into this project ,we got some problem of linking error.
It is possible to guide us how to insert a "SYS/BIOS" cfg file into this project? Does SYS/BIOS conflict with the XDCTOOL moudule already existing in the project "REL_210_V_H264_E_HP_DM365_02_00_00_11"?
2. Could we insert SYSTEM/BIOS moudules (SWI,task,....)just by inserting xdctool modules into cfg file without CCS4 environment ? ( for example :(var Task = xdc.useModule('ti.sysbios.knl.Task'))
3. Is it possible to guide us how to port a driver(for example : USB driver ) into the project REL_210_V_H264_E_HP_DM365_02_00_00_11? What Software framework should we follow?(for example Port the driver as a XDCTool moudule) ?
Any feedback with be appreciated
Best regards
Howl Cheng