Other Parts Discussed in Thread: DRA829
Hello everyone,
In order to increase the speed of OSPI FLASH data transmission, I need to adjust the clock provided to the flash to the maximum. At present, the flash I use is 1.8V, and the maximum SDR clock frequency is 200MHz. From the chip manual of DAR829, I know that DRA829 can provide 1.8V, and the maximum clock frequency of SDR is 133MHz. Does 133MHz here refer to the clock to the flash port after frequency division, or before the frequency division?
TI's demo program main_ospi_flash_test.c sets the OSPI clock to 133M in the INAC mode, but in OSPI_V0.c the open flash divides the clock by 32, so the divided clock is 4.2MHz, this value will be The clock frequency of the DRA829 is actually output to the flash port. I changed the frequency division factor to 4 and the flash will fail to open when the clock is 33.3MHz. I want to know what is the maximum frequency of DRA829 after crossover here?
Thank you!