Part Number: TDA4VMXEVM
Hi
I cannot find if there is optional EVM for CSI camera which can be connected to TDA4VMEVM.
How to get it?
Thanks and Best regards,
HaTa.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi HaTa,
Yes, you need to connect Fusion board and camera can be connected to fusion board.
Please refer to PSDKRA userguide for more details.
Rgds,
Brijesh
Hi Brijesh,
1) Where can I get (or buy) the Fusion board (Fusion serial capture board?) and camera module which can be connected to fusion board?
2) Are these board able to connected to all type of J7 EVM? (About the version of J7 EVM, please refer to my comment in "Notes" for this E2E thread)
Thanks and Best regards,
HaTa.
Hi HaTa,
You could buy fusion application board from spectrum digital and IMX390 camera from D3 (https://store.d3engineering.com/product/designcore-d3rcm-imx390-953-rugged-camera-module/)
There is only one type of J7 EVM, so yes it connects to this EVM.
Rgds,
Brijesh