Part Number: AM3358
Hello -
We have been working with the beaglebone black and I have a related question. the beaglebone uses gpio1_20 to reset the emmc as do we. I am trying to understand how this works. Since at boot all of the boot code (except the lowest level boot code ) lives in the emmc so in order to get the gpio pin out of its default mode which is low at reset of the processor, at some point the low level boot code in the sitara rom must release the gpio pin allowing it to go high. since the register setting for the gpios has not happened yet I am guessing the low level boot rom code configures the pins to be inputs and thus floating so the reset line is pulled up by an external pullup on the reset pin.
can you confirm this is what happens and could you suggest why it wouold not be better to control the emmc with the system reset on the board instead?
Thanks
Mark