Part Number: AM3354
Tool/software: Code Composer Studio
I use JTAG to test AM3354 and meet some problems.
My grogram named "Buzzer" comes from "StarterWare_02_00_01_01" . I connected the Target and load the GEL,then I load the program. the problem occured.
//
CortxA8: Breakpoint Manager: Retrying with a AET breakpoint
CortxA8: Trouble Setting Breakpoint with the Action "Semi hosting" at 0x8000****: (Error -1066 @ 0x333C) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 5.1.232.0)
//
If I ignored the warning and reload the program.the program would run some lines just like normal, but finally stop with the following warning.
//
CortxA8: Trouble Setting Breakpoint with the Action "Continue or Finish Stepping" at 0x80002d38: (Error -1066 @ 0x333C) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 8.4.0.00006)
CortxA8: Breakpoint Manager: Retrying with a AET breakpoint
//
What should I do to solve the problem?