This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

arm_a15_0: Trouble halting target cpu

Part Number: 66AK2H14

Tool/software: Code Composer Studio

while debugging u-boot, specifically ddr3_init, the program running away, the u-boot console did not go into wait-for-input mode,

to find out where the program is running at, i launch ccs930, plug in xds200 usb probe, load my ccxml, connect to arm_a15_0,

this is when "trouble halting target" occur. sometimes just one line, sometimes lots of them.

peculiarly, i can burn u-boot program into nor flash, printf messages shown in minicom proves that.

thanks in advance

johnthan