Hi, expert:
Are there any GEL files which can be used to check the CSI-TX functionality?
such as outputing color bar ?
This is to check the CSI-TX hardware functionality in the customer's new board.
Please kindly help.
btw, I can find a csitx->csirx test case in SDK6.2 TIOVX/kernel-j7/hwa/test. Do we need to connect the CSI-TX(DSI) output to CSI-RX to validate this case?
Please kindly share your comments.