This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: IPU2 availability for custom firmware

Part Number: AM5728

Hello,

We are proposing to use the SITARA AM57x cores in the following way:

  • SDK Linux running on Cortex-A.
  • SDK RTOS on the rest of the cores (Cortex-M and DSP C66x).

There is some controversy in the forum about whether it is possible to use the IPU2 (Cortex-M4) in applications that do not require multimedia support for IVA-HD. See below links:

https://e2e.ti.com/support/processors/f/791/t/586950

https://e2e.ti.com/support/processors/f/791/p/838347/3100896


In reply to Ahmad_Rashed:

I’ve asked around and found the answer is that we do not allow the IPU2 to be used for any purpose. The software teams will not support running your own firmware on the IPU2. It is however a separate subsystem from the IVA cores.

Best Regards, Mark P


Finally it is not clear if you can use the IPU2 for your own firmware or not. If possible, what would be the steps to be able to use it and avoid incompatibilities with the multimedia part of the Linux SDK?

Thanks a lot for for your support.

Best regards,

Gonzalo Vara