Other Parts Discussed in Thread: TVP7002
Hello,
I have found some posts similar to my issue, but I haven't been able to resolve my issue based on the answers found in other posts. I have the dm365 evm set up with the latest DVSDK (4.0) and I am having some issues running the encode demo. I have a camera hooked up to the composite input and when I run the encode demo, it seems to print some messages like:
EVM: switch to tvp7002 HD video input
... [omitted]
tvp7002 1-005c: querystd, errorxxx, val =1, val1 = 1
Error: Failed to create capture device
encode: linux/Fifo.c:177: Fifo_put: Assertion 'ptr' failed.
Aborted
From the messages, it seems like the encode demo is trying to operate on the component input and not the composite input. Is that accurate? If so, how do I get the encode demo to run on the composite input? Is there a different set of kernel command line parameters that I need to pass in via uboot?
As far as I know, I followed the steps in the user guide correctly and have everything set up correctly.
Any help would be greatly appreciated!