This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TDA2EVM5777: Where Can I get a default configuration file for TDA2EVM5777?

Part Number: TDA2EVM5777
Other Parts Discussed in Thread: TDA2

Tool/software: Code Composer Studio

Hello

I have a below board.

VAYA CPU BOARD ES2.0 GP / EVM5777BG-03-00-00 / TDA2EVM5777 

I think for operating board, I need a configuration file.

When after creating a CCS project, I think I have to "import" some zip file about board. (for memory, peripheral etc..)

I don't know how to say exactly, but you know what I'm saying.

(default configuration file / minimum configuration file maybe)

I installed PROCESSOR_SDK_VISION_03_07_00_00

Where Can I get an above-mentioned file(default configuration file)?

or Could you send me by email?

+) additionally,

when I create CCS project, on "Target" shell, I don't know what is my board type.

actually, I thought the board is TDA2x. so I chose target to "TDA2x", and the project example was "Hello World" in Basic Examples.

but the project didn't function.

so I chose another target "GPEVM_AM572X_SiRevA", then the project did function.

I wondering whether the target is TDA2x or GPEVM_AM572X_SiRevA.

Thank you

From. Kang

  • Hi,

    please check this Application Note:



    for debugging VisionSDK you can check "PROCESSOR_SDK_VISION_03_07_00_00/vision_sdk/docs/TrainingSlides/CCS_Debug_Trace.pdf"

    Regards,
    Yordan

  • Hello,

    In addition to what Yordan suggested, make sure you have also installed the device support package and emulation package on your CCS distribution (see automotive section since you have TDA2).

    https://software-dl.ti.com/ccs/esd/documents/ccs_device_support_files.html

    That will bring in what you call a "default" device target configuration option along with the basic gel initialization scripts and peripheral xmls. After which you should choose TDA2x and go with that. The AM572 is a very similar device to TDA2, so that's why it may be working, but it's for a different market and uses another SDK, so you should definitely use the proper part to use the Vision SDK going forward. 

    hope it helps,

    thanks,

    Alex

  • Thanks, I'll check that!

  • I did, but this problem has occurred

    and the code is a basic example "Hello World"

  • Can you re-attach the error screenshot? the image link is broken. 

    Are you able to connect to cores successfully? (without running any code yet)

    thanks,

    Alex

  • the first one is this

    and the second  one

    yep I connect core successfully

    and the first image is after connecting core and when load hello code (a.out)

  • OK, we have an article on this type of error. Please go through it and see if that helps.

    thanks,

    Alex

  • Thank you Alex!