Dear TI,
SW : psdk_rtos_auto_j7_06_02_00_21 + PSDKQA_7Q70.06.02
HW : TDA4VM EVM without INFOTAINMENT EXPANSION BOARD KIT.
When I try to run the "run_app_single_cam.sh", it seems like to working without error log. But eDP display is not working.
I already set the configuration for eDP display like below in "vision_apps/apps/basic_demos/app_tirtos/common/app_cfg_mcu2_1.h"
|
#define ENABLE_DSS #define ENABLE_DSS_SINGLE /* define below to enable eDP display, make sure to undef ENABLE_DSS_HDMI & ENABLE_DSS_DSI as well */ |
And this is uart logs
U-Boot SPL 2019.01-g350f3927b8 (Feb 17 2020 - 09:46:23 +0000)
SYSFW ABI: 2.9 (firmware rev 0x0013 '19.12.1-v2019.12a (Terrific Lla')
Trying to boot from MMC2
Loading Environment from MMC... *** Warning - No MMC card found, using default environment
Remoteproc 2 started successfully
** File not found /lib/firmware/j7-mcu-r5f0_0-fw **
Starting ATF on ARM64 core...
NOTICE: BL31: v2.2(release):ti2019.05-rc1
NOTICE: BL31: Built : 09:32:00, Feb 17 2020
I/TC:
I/TC: OP-TEE version: ti2019.05-rc1-dev (gcc version 8.3.0 (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36))) #1 Mon Feb 17 09:40:16 UTC 2020 aarch64
I/TC: Initialized
U-Boot SPL 2019.01-g350f3927b8 (Feb 17 2020 - 09:48:06 +0000)
Detected: J7X-BASE-CPB rev E3
Detected: J7X-VSC8514-ETH rev E2
Trying to boot from MMC2
U-Boot 2019.01-g350f3927b8 (Feb 17 2020 - 09:48:06 +0000)
SoC: J721E PG 1.0
Model: Texas Instruments K3 J721E SoC
Board: J721EX-PM2-SOM rev E7
DRAM: 4 GiB
Flash: 0 Bytes
MMC: sdhci@4f80000: 0, sdhci@4fb0000: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment
In: serial@2800000
Out: serial@2800000
Err: serial@2800000
Detected: J7X-BASE-CPB rev E3
Detected: J7X-VSC8514-ETH rev E2
Net:
Warning: ethernet@046000000 using MAC address from ROM
eth0: ethernet@046000000
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc1 is current device
SD/MMC found on device 1
** Unable to read file boot.scr **
98 bytes read in 1 ms (95.7 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc1 ...
Running uenvcmd ...
3807160 bytes read in 82 ms (44.3 MiB/s)
Load Remote Processor 3 with data@addr=0x80080000 3807160 bytes: Success!
** File not found /lib/firmware/j7-main-r5f1_0-fw **
1447952 bytes read in 33 ms (41.8 MiB/s)
Load Remote Processor 6 with data@addr=0x80080000 1447952 bytes: Success!
1447952 bytes read in 33 ms (41.8 MiB/s)
Load Remote Processor 7 with data@addr=0x80080000 1447952 bytes: Success!
6954352 bytes read in 63 ms (105.3 MiB/s)
Load Remote Processor 8 with data@addr=0x80080000 6954352 bytes: Success!
14281724 bytes read in 301 ms (45.2 MiB/s)
## Starting application at 0x80080000 ...
MMU: 16-bit ASID 44-bit PA TCR_EL1=b5183519
cpu0: MPIDR=80000000
cpu0: MIDR=411fd080 Cortex-A72 r1p0
cpu0: CWG=4 ERG=4 Dminline=4 Iminline=4 PIPT
cpu0: CLIDR=a200023 LoUU=1 LoC=2 LoUIS=1
cpu0: L1 Icache 48K linesz=64 set/way=256/3
cpu0: L1 Dcache 32K linesz=64 set/way=256/2
cpu0: L2 Unified 1024K linesz=64 set/way=1024/16
Loading IFS...done
cpu1: MPIDR=80000001
cpu1: MIDR=411fd080 Cortex-A72 r1p0
cpu1: CWG=4 ERG=4 Dminline=4 Iminline=4 PIPT
cpu1: CLIDR=a200023 LoUU=1 LoC=2 LoUIS=1
cpu1: L1 Icache 48K linesz=64 set/way=256/3
cpu1: L1 Dcache 32K linesz=64 set/way=256/2
cpu1: L2 Unified 1024K linesz=64 set/way=1024/16
System page at phys:0000000080011000 user:ffffff8040252000 kern:ffffff8040251000
Starting next program at vffffff8060084ae0
MMFLAGS=1
All ClockCycles offsets within tolerance
Welcome to QNX Neutrino 7.0 on TI J721E EVM Board!!
start serial driver
data: 4h ceh
Path=0 - am65x
target=0 lun=0 Direct-Access(0) - SDMMC: S0J56X Rev: 1.0
data: 7h fch
MASTER_SEND: Input/output error
Setting environment variables...
done..
Looking for user script to run: /sd/user.sh
Running user script...
user.sh called...
Setting additional environment variables...
Start sci res mgr..
Start shared memory allocator..
done...
J7EVM@QNX#
J7EVM@QNX#
J7EVM@QNX# slog2info
Jan 01 00:00:00.025 devb_sdmmc_am65x.8 slog* 1800 devb-sdmmc-am65x 1.00A (May 5 2020 13:47:53)
Jan 01 00:00:00.026 devb_sdmmc_am65x.8 slog 0 libcam.so (Aug 2 2019 15:41:15) bver 606010d
Jan 01 00:00:00.027 devb_sdmmc_am65x.8 slog 1800 sdio_cd: insertion path 0, cd state 0x1
Jan 01 00:00:00.028 devb_sdmmc_am65x.9 slog* 1800 devb-sdmmc-am65x 1.00A (May 5 2020 13:47:53)
Jan 01 00:00:00.029 devb_sdmmc_am65x.9 slog 0 libcam.so (Aug 2 2019 15:41:15) bver 606010d
Jan 01 00:00:00.030 devb_sdmmc_am65x.9 slog 1800 sdio_cd: insertion path 0, cd state 0x1
Jan 01 00:00:00.033 io_usb_otg.4106 slog* 0 main(447)[tid:1]: io-usb-otg (Nov 20 2019 16:51:50) args: -d xhci ioport=0x6010000,irq=128,iosize=65536,nousb3
Jan 01 00:00:00.036 io_usb_otg.4106 slog 0 xhci_controller_init(2607): devu-hcd-xhci.so (Nov 20 2019 16:42:36): args nousb3
Jan 01 00:00:00.036 io_usb_otg.4106 slog 8 usb_enum_port(92)[tid:1]: busno 0, parent -1, port 0, High speed
Jan 01 00:00:00.037 io_usb_otg.4106 slog 11 usb_client_descriptor_get(198)[tid:1]: (type 1, index 0, length 8)
Jan 01 00:00:00.037 io_usb_otg.4106 slog 12 usb_device_set_address(245)[tid:1]: b:0 devno 0
Jan 01 00:00:00.037 io_usb_otg.4106 slog 11 usb_client_descriptor_get(198)[tid:1]: (type 1, index 0, length 18)
Jan 01 00:00:00.037 io_usb_otg.4106 slog 11 usb_client_descriptor_get(198)[tid:1]: (type 2, index 0, length 9)
Jan 01 00:00:00.037 io_usb_otg.4106 slog 11 usb_client_descriptor_get(198)[tid:1]: (type 2, index 0, length 25)
Jan 01 00:00:00.037 io_usb_otg.4106 slog 8 usb_enum_port(139)[tid:1]: vid 0x0000, did 0x0000 enumerated(busno 0, devno 0:0)
Jan 01 00:00:00.037 io_usb_otg.4106 slog 11 hub_state_inserted(569)[tid:1]: bdentry 0, dentry 0 269635584
Jan 01 00:00:00.037 io_usb_otg.4106 slog 13 hub_configuration_enable(263)[tid:1]: 1
Jan 01 00:00:00.083 devb_sdmmc_am65x.9 slog 1800 SD CID:
Jan 01 00:00:00.083 devb_sdmmc_am65x.9 slog 1800 MID 0x3, OID 0x5344, PNM SL16G
Jan 01 00:00:00.083 devb_sdmmc_am65x.9 slog 1800 PRV 0x13, PSN 0xaf13bbaf, MDT 9-2019
Jan 01 00:00:00.083 devb_sdmmc_am65x.9 slog 1800 SD CSD:
Jan 01 00:00:00.083 devb_sdmmc_am65x.9 slog 1800 CSD_STRUCTURE 1, SPEC_VERS 0, CCC 0x5b5
Jan 01 00:00:00.083 devb_sdmmc_am65x.9 slog 1800 TAAC 14, NSAC 0, TRAN_SPEED 50
Jan 01 00:00:00.083 devb_sdmmc_am65x.9 slog 1800 C_SIZE 30386, C_SIZE_MULT 0
Jan 01 00:00:00.083 devb_sdmmc_am65x.9 slog 1800 READ_BL_LEN 9, WRITE_BL_LEN 9
Jan 01 00:00:00.083 devb_sdmmc_am65x.9 slog 1800 ERASE GRP_SIZE 0, GRP_MULT 0, SIZE 127
Jan 01 00:00:00.083 devb_sdmmc_am65x.9 slog 1800 blksz 512, sectors 31116288, dtr 25000000
Jan 01 00:00:00.083 devb_sdmmc_am65x.9 slog 1800 SD SW CAPS:
Jan 01 00:00:00.083 devb_sdmmc_am65x.9 slog 1800 bus mode 0x1f, cmd sys 0x1
Jan 01 00:00:00.083 devb_sdmmc_am65x.9 slog 1800 drv type 0xf, curr limit 0xf
Jan 01 00:00:00.083 devb_sdmmc_am65x.9 slog 1800 dtr 50000000
Jan 01 00:00:00.083 devb_sdmmc_am65x.9 slog 1800 CFG: Timing HS, DTR 50000000, Bus Width 4 bit
Jan 01 00:00:00.083 devb_sdmmc_am65x.9 slog 100 cam-disk.so (Aug 2 2019 15:41:25)
Jan 01 00:00:00.135 devb_sdmmc_am65x.8 slog 1800 MMC CID:
Jan 01 00:00:00.135 devb_sdmmc_am65x.8 slog 1800 MID 0x13, OID 0x4e, PNM S0J56X
Jan 01 00:00:00.135 devb_sdmmc_am65x.8 slog 1800 PRV 0x10, PSN 0x8c7c1ae, MDT 10-2018
Jan 01 00:00:00.135 devb_sdmmc_am65x.8 slog 1800 MMC CSD:
Jan 01 00:00:00.135 devb_sdmmc_am65x.8 slog 1800 CSD_STRUCTURE 3, SPEC_VERS 4, CCC 0x8f5
Jan 01 00:00:00.135 devb_sdmmc_am65x.8 slog 1800 TAAC 127, NSAC 1, TRAN_SPEED 50
Jan 01 00:00:00.135 devb_sdmmc_am65x.8 slog 1800 C_SIZE 4095, C_SIZE_MULT 7
Jan 01 00:00:00.135 devb_sdmmc_am65x.8 slog 1800 READ_BL_LEN 9, WRITE_BL_LEN 9
Jan 01 00:00:00.135 devb_sdmmc_am65x.8 slog 1800 ERASE GRP_SIZE 31, GRP_MULT 31, SIZE 0
Jan 01 00:00:00.135 devb_sdmmc_am65x.8 slog 1800 blksz 512, sectors 2097152, dtr 25000000
Jan 01 00:00:00.135 devb_sdmmc_am65x.8 slog 1800 MMC EXT CSD:
Jan 01 00:00:00.135 devb_sdmmc_am65x.8 slog 1800 DEVICE_TYPE 0x57, EXT_CSD_REV 8
Jan 01 00:00:00.135 devb_sdmmc_am65x.8 slog 1800 SEC_COUNT 31080448, dtr 200000000
Jan 01 00:00:00.135 devb_sdmmc_am65x.8 slog 1800 HC_ERASE_GRP_SIZE 1, HC_WP_GRP_SIZE 16
Jan 01 00:00:00.135 devb_sdmmc_am65x.8 slog 1800 STROBE 0x0, BKOPS_EN 0x0
Jan 01 00:00:00.135 devb_sdmmc_am65x.8 slog 1800 Driver type: 0x0
Jan 01 00:00:00.135 devb_sdmmc_am65x.8 slog 1800 CFG: Timing HS400, DTR 200000000, Bus Width 8 bit
Jan 01 00:00:00.135 devb_sdmmc_am65x.8 slog 100 cam-disk.so (Aug 2 2019 15:41:25)
Jan 01 00:00:00.141 io_usb_otg.4106 slog 0 usbh_timeout_init(203)[tid:1]: Complete
Jan 01 00:00:00.146 io_usb_otg.4106 slog 0 usbh_bus_status_update(309)[tid:1]: busno 0, value = 0 critical error reported
Jan 01 00:00:00.146 io_usb_otg.4106 slog 8 usb_enum_port_extract(170)[tid:7]: (busno 0, pdevno 0, portno 1)
Jan 01 00:00:00.146 io_usb_otg.4106 slog 8 usb_enum_port_extract(190)[tid:7]: status (2)
Jan 01 00:00:00.461 shmemallocator.20493 slog* 0 SharedMemoryAllocator: BaseAddress: 0xae000000 Size: 0x20000000 (536870912)
Jan 01 00:00:00.461 shmemallocator.20493 slog 0 SharedMemoryAllocator: BaseAddress: 0x00000000 Size: 0x00000000 (0)
J7EVM@QNX#
J7EVM@QNX#
J7EVM@QNX# cd sd/vision_apps/
J7EVM@QNX# ./vision_apps_init.sh
J7EVM@QNX# APP_LOG: Mapping ac000000 ...
APP_LOG: Mapped ac000000 -> 28000000 of size 262144 bytes
[MCU2_1] 0.000460 s: CIO: Init ... Done !!!
[MCU2_1] 0.000529 s: ### CPU Frequency <ORG = 1000000000 Hz>, <NEW = 1000000000 Hz>
[MCU2_1] 0.000572 s: APP: Init ... !!!
[MCU2_1] 0.000590 s: SCICLIENT: Init ... !!!
[MCU2_1] 0.003820 s: SCICLIENT: DMSC FW version [19.12.1-v
19.12a (Terrific Lla]
[MCU2_1] 0.003868 s: SCICLIENT: DMSC FW revision 0x13
[MCU2_1] 0.003892 s: SCICLIENT: DMSC FW ABI revision 2.9
[MCU2_1] 0.003916 s: SCICLIENT: Init ... Done !!!
[MCU2_1] 0.003938 s: UDMA: Init ... !!!
[MCU2_1] 0.070775 s: UDMA: Init ... Done !!!
[MCU2_1] 0.070822 s: MEM: Init ... !!!
[MCU2_1] 0.070857 s: MEM: Created heap (DDR_SHARED_MEM, id=0, flags=0x00000004) @ d2c00000 of size 16777216 bytes !!!
[MCU2_1] 0.070911 s: MEM: Created heap (DDR_NON_CACHE_ME, id=5, flags=0x00000000) @ ce000000 of size 67108864 bytes !!!
[MCU2_1] 0.070956 s: MEM: Init ... Done !!!
[MCU2_1] 0.070975 s: IPC: Init ... !!!
[MCU2_1] 0.071004 s: IPC: 5 CPUs participating in IPC !!!
[MCU2_1] 0.173157 s: IPC: Init ... Done !!!
[MCU2_1] 0.173213 s: APP: Syncing with 4 CPUs ... !!!
[MCU2_1] 1.280261 s: APP: Syncing with 4 CPUs ... Done !!!
[MCU2_1] 1.280432 s: REMOTE_SERVICE: Init ... !!!
[MCU2_1] 1.281616 s: REMOTE_SERVICE: Init ... Done !!!
[MCU2_1] 1.281679 s: FVID2: Init ... !!!
[MCU2_1] 1.281748 s: FVID2: Init ... Done !!!
[MCU2_1] 1.281794 s: DSS: Init ... !!!
[MCU2_1] 1.281818 s: DSS: Display type is eDP !!!
[MCU2_1] 1.281839 s: DSS: SoC init ... !!!
[MCU2_1] 1.281859 s: SCICLIENT: Sciclient_pmSetModuleState module=152 state=2
[MCU2_1] 1.302495 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_1] 1.302558 s: SCICLIENT: Sciclient_pmSetModuleState module=297 state=2
[MCU2_1] 1.383712 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_1] 1.383744 s: SCICLIENT: Sciclient_pmSetModuleState module=151 state=2
[MCU2_1] 1.420196 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_1] 1.420225 s: SCICLIENT: Sciclient_pmSetModuleClkParent module=152 clk=9 parent=11
[MCU2_1] 1.450952 s: SCICLIENT: Sciclient_pmSetModuleClkParent success
[MCU2_1] 1.450984 s: SCICLIENT: Sciclient_pmSetModuleClkParent module=152 clk=13 parent=18
[MCU2_1] 1.485183 s: SCICLIENT: Sciclient_pmSetModuleClkParent success
[MCU2_1] 1.485213 s: SCICLIENT: Sciclient_pmSetModuleClkParent module=152 clk=1 parent=2
[MCU2_1] 1.539444 s: SCICLIENT: Sciclient_pmSetModuleClkParent success
[MCU2_1] 1.539474 s: SCICLIENT: Sciclient_pmSetModuleClkFreq module=152 clk=1 freq=148500000
[MCU2_1] 1.587378 s: SCICLIENT: Sciclient_pmSetModuleClkFreq success
[MCU2_1] 1.587408 s: SCICLIENT: Sciclient_pmModuleClkRequest module=152 clk=1 state=2 flag=0
[MCU2_1] 1.643403 s: SCICLIENT: Sciclient_pmModuleClkRequest success
[MCU2_1] 1.643432 s: DSS: SoC init ... Done !!!
[MCU2_1] 1.643469 s: src/drv/common/dss_init.c @ Line 99:
[MCU2_1] 1.643495 s: [JWD ***]Dss_init start
[MCU2_1] 1.643552 s: [JWD] Dss_fillSocInfo
[MCU2_1] 1.643599 s: [JWD] Dss_fillSocInfo : isCommRegAvailable[0]
[MCU2_1] 1.643646 s: [JWD] Dss_fillSocInfo : isPipeAvailable[0]
[MCU2_1] 1.643687 s: [JWD] Dss_fillSocInfo : isPipeAvailable[1]
[MCU2_1] 1.643726 s: [JWD] Dss_fillSocInfo : isPipeAvailable[2]
[MCU2_1] 1.643768 s: [JWD] Dss_fillSocInfo : isOverlayAvailable TRUE++[0]
[MCU2_1] 1.643811 s: [JWD] Dss_fillSocInfo : isOverlayAvailable FALSE--
[MCU2_1] 1.643851 s: [JWD] Dss_fillSocInfo : isOverlayAvailable FALSE--
[MCU2_1] 1.643890 s: [JWD] Dss_fillSocInfo : isOverlayAvailable FALSE--
[MCU2_1] 1.643930 s: [JWD] Dss_fillSocInfo : isPortAvailable[0]
[MCU2_1] 1.660011 s: [JWD] DCTRL: appDctrlInit!!!
[MCU2_1] 1.660085 s: [JWD] DCTRL: appDctrlControl cmd = 0x1
[MCU2_1] 1.660123 s: [JWD] DCTRL: appDctrlRegisterHandleCmd
[MCU2_1] 1.660159 s: [JWD] DCTRL: doHpd enabled
[MCU2_1] 1.660222 s: [JWD] DCTRL: doHpd enabled:IOCTL_DSS_DCTRL_REGISTER_DP_HPD_CB
[MCU2_1] 1.660275 s: src/drv/dctrl/dss_dctrlApi.c @ Line 746:
[MCU2_1] 1.660304 s: [JWD]Dss_dctrlDrvControl start
[MCU2_1] 1.660351 s: [JWD ***] Dss_dctrlDrvSetDpHpdCbParamsIoctl
[MCU2_1] 1.660398 s: [JWD] DCTRL: appDctrlControl cmd = 0x3
[MCU2_1] 1.660429 s: [JWD] DCTRL: appDctrlSetPathCmd
[MCU2_1] 1.660458 s: src/drv/dctrl/dss_dctrlApi.c @ Line 746:
[MCU2_1] 1.660484 s: [JWD]Dss_dctrlDrvControl start
[MCU2_1] 1.660645 s: [JWD] DCTRL: appDctrlControl cmd = 0x5
[MCU2_1] 1.660689 s: [JWD] DCTRL: appDctrlSetVpParamsCmd
[MCU2_1] 1.660727 s: src/drv/dctrl/dss_dctrlApi.c @ Line 746:
[MCU2_1] 1.660755 s: [JWD]Dss_dctrlDrvControl start
[MCU2_1] 1.660796 s: [JWD] IOCTL_DSS_DCTRL_SET_VP_PARAMS ***
[MCU2_1] 1.660895 s: [JWD ***]Dss_dctrlDrvIsOutputDP : vpFound = 1, vpId = 0
[MCU2_1] 1.660943 s: [JWD] DCTRL: appDctrlControl cmd = 0x9
[MCU2_1] 1.660978 s: [JWD] DCTRL: appDctrlSetAdvVpParamsCmd
[MCU2_1] 1.661010 s: src/drv/dctrl/dss_dctrlApi.c @ Line 746:
[MCU2_1] 1.661037 s: [JWD]Dss_dctrlDrvControl start
[MCU2_1] 1.661067 s: [JWD] DCTRL: appDctrlControl cmd = 0x6
[MCU2_1] 1.661095 s: [JWD] DCTRL: appDctrlSetOverlayParamsCmd
[MCU2_1] 1.661125 s: src/drv/dctrl/dss_dctrlApi.c @ Line 746:
[MCU2_1] 1.661150 s: [JWD]Dss_dctrlDrvControl start
[MCU2_1] 1.661187 s: [JWD] IOCTL_DSS_DCTRL_SET_OVERLAY_PARAMS ***
[MCU2_1] 1.661227 s: [JWD] DCTRL: appDctrlControl cmd = 0x7
[MCU2_1] 1.661257 s: [JWD***] appDctrlSetLayerParamsCmd : overlayId=0
[MCU2_1] 1.661285 s: [JWD***] appDctrlSetLayerParamsCmd : pipeLayerNum[0]=0
[MCU2_1] 1.661314 s: [JWD***] appDctrlSetLayerParamsCmd : pipeLayerNum[1]=4
[MCU2_1] 1.661344 s: [JWD***] appDctrlSetLayerParamsCmd : pipeLayerNum[2]=1
[MCU2_1] 1.661372 s: [JWD***] appDctrlSetLayerParamsCmd : pipeLayerNum[3]=255
[MCU2_1] 1.661407 s: src/drv/dctrl/dss_dctrlApi.c @ Line 746:
[MCU2_1] 1.661432 s: [JWD]Dss_dctrlDrvControl start
[MCU2_1] 1.661479 s: [JWD***]Dss_dctrlDrvSetLayerParamsIoctl, overlayRegs = 0x4a70000
[MCU2_1] 1.661573 s: [JWD---]regVal = 0x0, inputPipe=0, layerEnable=1, layerNum=0
[MCU2_1] 1.661631 s: [JWD] CSL_dssOverlaySetLayerConfig ======== final regVal=0x1
[MCU2_1] 1.661685 s: [JWD---]regVal = 0x0, inputPipe=1, layerEnable=1, layerNum=4
[MCU2_1] 1.661735 s: [JWD] CSL_dssOverlaySetLayerConfig ======== final regVal=0x3
[MCU2_1] 1.661785 s: [JWD---]regVal = 0x0, inputPipe=2, layerEnable=1, layerNum=1
[MCU2_1] 1.661833 s: [JWD] CSL_dssOverlaySetLayerConfig ======== final regVal=0x5
[MCU2_1] 1.661866 s: DSS: Init ... Done !!!
[MCU2_1] 1.661887 s: VHWA: Init ... !!!
[MCU2_1] 1.661905 s: SCICLIENT: Sciclient_pmSetModuleState module=290 state=2
[MCU2_1] 1.705402 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_1] 1.705451 s: SCICLIENT: Sciclient_pmSetModuleState module=48 state=2
[MCU2_1] 1.726220 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_1] 1.726258 s: SCICLIENT: Sciclient_pmSetModuleState module=305 state=2
[MCU2_1] 1.741719 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_1] 1.741751 s: VHWA: DOF Init ... !!!
[MCU2_1] 2.783015 s: VHWA: DOF Init ... Done !!!
[MCU2_1] 2.783071 s: VHWA: LDC Init ... !!!
[MCU2_1] 3.240808 s: VHWA: LDC Init ... Done !!!
[MCU2_1] 3.240861 s: VHWA: MSC Init ... !!!
[MCU2_1] 4.611097 s: VHWA: MSC Init ... Done !!!
[MCU2_1] 4.611151 s: VHWA: NF Init ... !!!
[MCU2_1] 4.839190 s: VHWA: NF Init ... Done !!!
[MCU2_1] 4.839239 s: VHWA: SDE Init ... !!!
[MCU2_1] 5.183021 s: VHWA: SDE Init ... Done !!!
[MCU2_1] 5.183074 s: VHWA: VISS Init ... !!!
[MCU2_1] 6.210678 s: VHWA: VISS Init ... Done !!!
[MCU2_1] 6.210730 s: VHWA: VDEC Init ... !!!
[MCU2_1] 6.232906 s: VHWA: VDEC Init ... Done !!!
[MCU2_1] 6.232958 s: VHWA: VENC Init ... !!!
[MCU2_1] 6.285833 s: VHWA: VENC Init ... Done !!!
[MCU2_1] 6.285889 s: VHWA: Init ... Done !!!
[MCU2_1] 6.285925 s: VX_ZONE_INIT:Enabled
[MCU2_1] 6.285949 s: VX_ZONE_ERROR:Enabled
[MCU2_1] 6.285969 s: VX_ZONE_WARNING:Enabled
[MCU2_1] 6.288625 s: VX_ZONE_ERROR:[tivxTargetCreate:1260] tivxTargetCreate: target is NULL
[MCU2_1] 6.288683 s: VX_ZONE_ERROR:[tivxPlatformCreateTargetId:48] Could not Add Target
[MCU2_1] 6.288730 s: VX_ZONE_INIT:[tivxInit:64] Initialization Done !!!
[MCU2_1] 6.288758 s: APP: OpenVX Target kernel init ... !!!
[MCU2_1] 6.295347 s: APP: OpenVX Target kernel init ... Done !!!
[MCU2_1] 6.295398 s: CSI2RX: Init ... !!!
[MCU2_1] 6.295419 s: SCICLIENT: Sciclient_pmSetModuleState module=25 state=2
[MCU2_1] 6.299816 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_1] 6.299859 s: SCICLIENT: Sciclient_pmSetModuleState module=26 state=2
[MCU2_1] 6.311843 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_1] 6.311872 s: SCICLIENT: Sciclient_pmSetModuleState module=27 state=2
[MCU2_1] 6.323902 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_1] 6.323935 s: SCICLIENT: Sciclient_pmSetModuleState module=147 state=2
[MCU2_1] 6.332096 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_1] 6.332126 s: SCICLIENT: Sciclient_pmSetModuleState module=148 state=2
[MCU2_1] 6.340329 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_1] 6.386870 s: CSI2RX: Init ... Done !!!
[MCU2_1] 6.386916 s: CSI2TX: Init ... !!!
[MCU2_1] 6.386939 s: SCICLIENT: Sciclient_pmSetModuleState module=25 state=2
[MCU2_1] 6.391289 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_1] 6.391321 s: SCICLIENT: Sciclient_pmSetModuleState module=28 state=2
[MCU2_1] 6.404316 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_1] 6.404349 s: SCICLIENT: Sciclient_pmSetModuleState module=296 state=2
[MCU2_1] 6.415366 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU2_1] 6.461811 s: CSI2TX: Init ... Done !!!
[MCU2_1] 6.461853 s: ISS: Init ... !!!
[MCU2_1] 6.461913 s: Found sensor IMX390-UB953_D3 at location 0
[MCU2_1] 6.461965 s: Found sensor AR0233-UB953_MARS at location 1
[MCU2_1] 6.462008 s: Found sensor AR0820-UB953_LI at location 2
[MCU2_1] 6.462035 s: ISS: Init ... Done !!!
[MCU2_1] 6.462059 s: UDMA Copy: Init ... !!!
[MCU2_1] 6.725290 s: UDMA Copy: Init ... Done !!!
[MCU2_1] 6.725343 s: APP: Init ... Done !!!
[MCU2_1] 6.725372 s: APP: Run ... !!!
[MCU2_1] 6.725391 s: IPC: Starting echo test ...
[MCU2_1] 6.727146 s: APP: Run ... Done !!!
[MCU2_1] 6.728267 s: IPC: Echo status: mpu1_0[x] mcu2_1[s] C66X_1[.] C66X_2[P] C7X_1[.]
[MCU2_1] 6.728431 s: IPC: Echo status: mpu1_0[x] mcu2_1[s] C66X_1[P] C66X_2[P] C7X_1[.]
[MCU2_1] 6.728509 s: IPC: Echo status: mpu1_0[x] mcu2_1[s] C66X_1[P] C66X_2[P] C7X_1[P]
[C6x_1 ] 0.026462 s: CIO: Init ... Done !!!
[C6x_1 ] 0.026495 s: ### CPU Frequency <ORG = 1350000000 Hz>, <NEW = 1350000000 Hz>
[C6x_1 ] 0.026508 s: APP: Init ... !!!
[C6x_1 ] 0.026515 s: SCICLIENT: Init ... !!!
[C6x_1 ] 0.031428 s: SCICLIENT: DMSC FW version [19.12.1-v
19.12a (Terrific Lla]
[C6x_1 ] 0.031440 s: SCICLIENT: DMSC FW revision 0x13
[C6x_1 ] 0.031448 s: SCICLIENT: DMSC FW ABI revision 2.9
[C6x_1 ] 0.031458 s: SCICLIENT: Init ... Done !!!
[C6x_1 ] 0.031467 s: UDMA: Init ... !!!
[C6x_1 ] 0.138202 s: UDMA: Init ... Done !!!
[C6x_1 ] 0.138220 s: MEM: Init ... !!!
[C6x_1 ] 0.138232 s: MEM: Created heap (DDR_SHARED_MEM, id=0, flags=0x00000004) @ d4000000 of size 16777216 bytes !!!
[C6x_1 ] 0.138249 s: MEM: Created heap (L2_MEM, id=2, flags=0x00000001) @ 800000 of size 229376 bytes !!!
[C6x_1 ] 0.138264 s: MEM: Created heap (DDR_SCRATCH_MEM, id=4, flags=0x00000001) @ d5000000 of size 50331648 bytes !!!
[C6x_1 ] 0.138279 s: MEM: Init ... Done !!!
[C6x_1 ] 0.138287 s: IPC: Init ... !!!
[C6x_1 ] 0.138300 s: IPC: 5 CPUs participating in IPC !!!
[C6x_1 ] 0.436144 s: IPC: Init ... Done !!!
[C6x_1 ] 0.436173 s: APP: Syncing with 4 CPUs ... !!!
[C6x_1 ] 1.082766 s: APP: Syncing with 4 CPUs ... Done !!!
[C6x_1 ] 1.082777 s: REMOTE_SERVICE: Init ... !!!
[C6x_1 ] 1.083400 s: REMOTE_SERVICE: Init ... Done !!!
[C6x_1 ] 1.083441 s: VX_ZONE_INIT:Enabled
[C6x_1 ] 1.083451 s: VX_ZONE_ERROR:Enabled
[C6x_1 ] 1.083461 s: VX_ZONE_WARNING:Enabled
[C6x_1 ] 1.084250 s: VX_ZONE_INIT:[tivxInit:64] Initialization Done !!!
[C6x_1 ] 1.084268 s: APP: OpenVX Target kernel init ... !!!
[C6x_1 ] 1.084490 s: APP: OpenVX Target kernel init ... Done !!!
[C6x_1 ] 1.084508 s: APP: Init ... Done !!!
[C6x_1 ] 1.084516 s: APP: Run ... !!!
[C6x_1 ] 1.084524 s: IPC: Starting echo test ...
[C6x_1 ] 1.085389 s: APP: Run ... Done !!!
[C6x_1 ] 1.085650 s: IPC: Echo status: mpu1_0[x] mcu2_1[x] C66X_1[s] C66X_2[x] C7X_1[P]
[C6x_1 ] 1.494461 s: IPC: Echo status: mpu1_0[x] mcu2_1[x] C66X_1[s] C66X_2[P] C7X_1[P]
[C6x_1 ] 6.530614 s: IPC: Echo status: mpu1_0[x] mcu2_1[P] C66X_1[s] C66X_2[P] C7X_1[P]
[C6x_2 ] 0.024931 s: CIO: Init ... Done !!!
[C6x_2 ] 0.024965 s: ### CPU Frequency <ORG = 1350000000 Hz>, <NEW = 1350000000 Hz>
[C6x_2 ] 0.024978 s: APP: Init ... !!!
[C6x_2 ] 0.024985 s: SCICLIENT: Init ... !!!
[C6x_2 ] 0.028168 s: SCICLIENT: DMSC FW version [19.12.1-v
19.12a (Terrific Lla]
[C6x_2 ] 0.028180 s: SCICLIENT: DMSC FW revision 0x13
[C6x_2 ] 0.028189 s: SCICLIENT: DMSC FW ABI revision 2.9
[C6x_2 ] 0.028198 s: SCICLIENT: Init ... Done !!!
[C6x_2 ] 0.028206 s: UDMA: Init ... !!!
[C6x_2 ] 0.134953 s: UDMA: Init ... Done !!!
[C6x_2 ] 0.134977 s: MEM: Init ... !!!
[C6x_2 ] 0.134989 s: MEM: Created heap (DDR_SHARED_MEM, id=0, flags=0x00000004) @ d8000000 of size 16777216 bytes !!!
[C6x_2 ] 0.135007 s: MEM: Created heap (L2_MEM, id=2, flags=0x00000001) @ 800000 of size 229376 bytes !!!
[C6x_2 ] 0.135021 s: MEM: Created heap (DDR_SCRATCH_MEM, id=4, flags=0x00000001) @ d9000000 of size 50331648 bytes !!!
[C6x_2 ] 0.135036 s: MEM: Init ... Done !!!
[C6x_2 ] 0.135044 s: IPC: Init ... !!!
[C6x_2 ] 0.135057 s: IPC: 5 CPUs participating in IPC !!!
[C6x_2 ] 0.434489 s: IPC: Init ... Done !!!
[C6x_2 ] 0.434521 s: APP: Syncing with 4 CPUs ... !!!
[C6x_2 ] 0.619633 s: APP: Syncing with 4 CPUs ... Done !!!
[C6x_2 ] 0.619643 s: REMOTE_SERVICE: Init ... !!!
[C6x_2 ] 0.620266 s: REMOTE_SERVICE: Init ... Done !!!
[C6x_2 ] 0.620307 s: VX_ZONE_INIT:Enabled
[C6x_2 ] 0.620317 s: VX_ZONE_ERROR:Enabled
[C6x_2 ] 0.620325 s: VX_ZONE_WARNING:Enabled
[C6x_2 ] 0.621100 s: VX_ZONE_INIT:[tivxInit:64] Initialization Done !!!
[C6x_2 ] 0.621117 s: APP: OpenVX Target kernel init ... !!!
[C6x_2 ] 0.621350 s: APP: OpenVX Target kernel init ... Done !!!
[C6x_2 ] 0.621369 s: UDMA Copy: Init ... !!!
[C6x_2 ] 1.030091 s: UDMA Copy: Init ... Done !!!
[C6x_2 ] 1.030112 s: APP: Init ... Done !!!
[C6x_2 ] 1.030119 s: APP: Run ... !!!
[C6x_2 ] 1.030127 s: IPC: Starting echo test ...
[C6x_2 ] 1.031033 s: APP: Run ... Done !!!
[C6x_2 ] 1.031337 s: IPC: Echo status: mpu1_0[x] mcu2_1[x] C66X_1[P] C66X_2[s] C7X_1[.]
[C6x_2 ] 1.031372 s: IPC: Echo status: mpu1_0[x] mcu2_1[x] C66X_1[P] C66X_2[s] C7X_1[P]
[C6x_2 ] 6.067502 s: IPC: Echo status: mpu1_0[x] mcu2_1[P] C66X_1[P] C66X_2[s] C7X_1[P]
[C7x_1 ] 0.011700 s: CIO: Init ... Done !!!
[C7x_1 ] 0.011723 s: ### CPU Frequency <ORG = 1000000000 Hz>, <NEW = 1000000000 Hz>
[C7x_1 ] 0.011740 s: APP: Init ... !!!
[C7x_1 ] 0.011748 s: SCICLIENT: Init ... !!!
[C7x_1 ] 0.014926 s: SCICLIENT: DMSC FW version [19.12.1-v
19.12a (Terrific Lla]
[C7x_1 ] 0.014941 s: SCICLIENT: DMSC FW revision 0x13
[C7x_1 ] 0.014951 s: SCICLIENT: DMSC FW ABI revision 2.9
[C7x_1 ] 0.014961 s: SCICLIENT: Init ... Done !!!
[C7x_1 ] 0.014971 s: UDMA: Init ... !!!
[C7x_1 ] 0.033642 s: UDMA: Init ... Done !!!
[C7x_1 ] 0.033653 s: MEM: Init ... !!!
[C7x_1 ] 0.033665 s: MEM: Created heap (DDR_SHARED_MEM, id=0, flags=0x00000004) @ dc000000 of size 469762048 bytes !!!
[C7x_1 ] 0.033685 s: MEM: Created heap (L3_MEM, id=1, flags=0x00000001) @ 70020000 of size 8159232 bytes !!!
[C7x_1 ] 0.033703 s: MEM: Created heap (L2_MEM, id=2, flags=0x00000001) @ 64800000 of size 491520 bytes !!!
[C7x_1 ] 0.033720 s: MEM: Created heap (L1_MEM, id=3, flags=0x00000001) @ 64e00000 of size 16384 bytes !!!
[C7x_1 ] 0.033745 s: MEM: Created heap (DDR_SCRATCH_MEM, id=4, flags=0x00000001) @ f8000000 of size 67108864 bytes !!!
[C7x_1 ] 0.033763 s: MEM: Init ... Done !!!
[C7x_1 ] 0.033771 s: IPC: Init ... !!!
[C7x_1 ] 0.033781 s: IPC: 5 CPUs participating in IPC !!!
[C7x_1 ] 0.178289 s: IPC: Init ... Done !!!
[C7x_1 ] 0.178302 s: APP: Syncing with 4 CPUs ... !!!
[C7x_1 ] 0.178316 s: APP: Syncing with 4 CPUs ... Done !!!
[C7x_1 ] 0.178327 s: REMOTE_SERVICE: Init ... !!!
[C7x_1 ] 0.178561 s: REMOTE_SERVICE: Init ... Done !!!
[C7x_1 ] 0.178582 s: VX_ZONE_INIT:Enabled
[C7x_1 ] 0.178593 s: VX_ZONE_ERROR:Enabled
[C7x_1 ] 0.178602 s: VX_ZONE_WARNING:Enabled
[C7x_1 ] 0.178843 s: VX_ZONE_INIT:[tivxInit:64] Initialization Done !!!
[C7x_1 ] 0.178856 s: APP: OpenVX Target kernel init ... !!!
[C7x_1 ] 0.178927 s: APP: OpenVX Target kernel init ... Done !!!
[C7x_1 ] 0.178941 s: APP: Init ... Done !!!
[C7x_1 ] 0.178950 s: APP: Run ... !!!
[C7x_1 ] 0.178959 s: IPC: Starting echo test ...
[C7x_1 ] 0.179358 s: APP: Run ... Done !!!
[C7x_1 ] 0.181211 s: IPC: Echo status: mpu1_0[x] mcu2_1[x] C66X_1[P] C66X_2[x] C7X_1[s]
[C7x_1 ] 0.590022 s: IPC: Echo status: mpu1_0[x] mcu2_1[x] C66X_1[P] C66X_2[P] C7X_1[s]
[C7x_1 ] 5.626208 s: IPC: Echo status: mpu1_0[x] mcu2_1[P] C66X_1[P] C66X_2[P] C7X_1[s]
J7EVM@QNX#
J7EVM@QNX#
J7EVM@QNX# ./run_app_single_cam.sh
APP: Init QNX ... !!!
APP_LOG: Mapping ac000000 ...
APP_LOG: Mapped ac000000 -> 28000000 of size 262144 bytes
appIpcInit: IPC: Init QNX ... !!!
IPC: 5 CPUs participating in IPC !!!
ti_sci_msg_xfer: ACK error
Mailbox_plugInterrupt: interrupt Number 123, arg 0x10489D98
ti_sci_msg_xfer: ACK error
Mailbox_plugInterrupt: interrupt Number 124, arg 0x10489F30
ti_sci_msg_xfer: ACK error
Mailbox_plugInterrupt: interrupt Number 125, arg 0x1048A0C8
appIpcInit: IPC: Init ... Done !!!
0.000000 s: REMOTE_SERVICE: Init ... !!!
0.000000 s: REMOTE_SERVICE: Init ... Done !!!
APP: Init ... Done !!!
0.000000 s: VX_ZONE_INIT:Enabled
0.000000 s: VX_ZONE_ERROR:Enabled
0.000000 s: VX_ZONE_WARNING:Enabled
0.000000 s: VX_ZONE_INIT:[tivxInit:64] Initialization Done !!!
0.000000 s: VX_ZONE_INIT:[tivxHostInit:44] Initialization Done for HOST !!!
Invalid token [
]
sensor_selection = [0]
Invalid token [
]
ldc_enable = [0]
Invalid token [
]
num_frames_to_run = [1000000000]
Invalid token [
]
is_interactive = [1]
tivxImagingLoadKernels done
0.005000 s: ISS: Enumerating sensors ... !!!
0.005000 s: ISS: Enumerating sensors ... found 0 : IMX390-UB953_D3
0.005000 s: ISS: Enumerating sensors ... found 1 : AR0233-UB953_MARS
0.005000 s: ISS: Enumerating sensors ... found 2 : AR0820-UB953_LI
3 sensor(s) found
Supported sensor list:
[MCU2_1] 30.451564 s: ImageSensor_RemoteServiceHandler: IM_SENSOR_CMD_CREATE
a : IMX390-UB953_D3
[MCU2_1] 30.451622 s: Sensor at index 0 = IMX390-UB953_D3
b : AR0233-UB953_MARS
[MCU2_1] 30.451653 s: Sensor at index 1 = AR0233-UB953_MARS
c : AR0820-UB953_LI
[MCU2_1] 30.451679 s: Sensor at index 2 = AR0820-UB953_LI
Select a sensor
a
LDC Selection Yes(1)/No(0)
LDC Selection Yes(1)/No(0)
0
Sensor selected : IMX390-UB953_D3
app_init done
Querying IMX390-UB953_D3
2.371000 s: ISS: Querying sensor [IMX390-UB953_D3] ... !!!
2.371000 s: ISS: Querying sensor [IMX390-UB953_D3] ... Done !!!
WDR mode is supported
Expsoure control is supported
Gain control is supported
CMS Usecase is supported
Sensor width = 1936
Sensor height = 1096
Sensor DCC ID = 390
Sensor Supported Features = 0x378
Sensor Enabled Features = 0x358
2.371000 s: ISS: Initializing sensor [IMX390-UB953_D3], doing IM_SENSOR_CMD_PWRON ... !!!
[MCU2_1] 32.817526 s: ImageSensor_RemoteServiceHandler: IM_SENSOR_CMD_QUERY
[MCU2_1] 32.817589 s: Received Query for IMX390-UB953_D3
[MCU2_1] 32.817912 s: ImageSensor_RemoteServiceHandler: IM_SENSOR_CMD_PWRON
[MCU2_1] 32.817985 s: IM_SENSOR_CMD_PWRON : channel_mask = 0x1
[MCU2_1] 32.818108 s: IMX390_PowerOn : chMask = 0x1
[MCU2_1] 32.818161 s: ub960_cfgScript : ub960I2cAddr = 0x3d
[MCU2_1] 32.818189 s: UB960 config start
7.203000 s: ISS: Initializing sensor [IMX390-UB953_D3], doing IM_SENSOR_CMD_CONFIG ... !!!
[MCU2_1] 37.649616 s: End of UB960 config
[MCU2_1] 37.649909 s: ImageSensor_RemoteServiceHandler: IM_SENSOR_CMD_CONFIG
[MCU2_1] 37.649956 s: Application requested features = 0x358
[MCU2_1]
[MCU2_1] 37.650019 s: ub960_cfgScript : ub960I2cAddr = 0x3d
[MCU2_1] 37.650053 s: UB960 config start
[MCU2_1] 37.889615 s: End of UB960 config
[MCU2_1] 37.889659 s: Configuring camera # 0
[MCU2_1] 37.889688 s: ub953 config start : slaveAddr = 0x74
[MCU2_1] 38.256626 s: End of UB953 config
[MCU2_1] 38.256700 s: Configuring IMX390 imager 0x40.. Please wait till it finishes
9.969000 s: ISS: Initializing sensor [IMX390-UB953_D3] ... Done !!!
Creating graph
Initializing params for capture node
Initializing params for capture node
local_capture_config.numDataLanes = 4
local_capture_config.dataLanesMap[0] = 1
local_capture_config.dataLanesMap[1] = 2
local_capture_config.dataLanesMap[2] = 3
local_capture_config.dataLanesMap[3] = 4
capture_config = 0x1034a4c0
Creating capture node
obj->capture_node = 0x1031dec0
VISS Set Reference done
AEWB Set Reference done
Display Set Target done
vxSetGraphScheduleConfig done
[MCU2_1] 40.415557 s: IMX390 config done
[MCU2_1] 40.415607 s: IM_SENSOR_CMD_CONFIG returning status = 0
Scaler is enabled
[MCU2_1] 41.519294 s: [JWD] Dss_dispDrvSetDssParamsIoctl : overlayRegs = 0x4a70000
[MCU2_1] 41.519382 s: [JWD]-pdk [0]regVal = 0x1, enble = 0x1, inputPipe = 0x0, pipeId = 0x2
[MCU2_1] 41.519444 s: [JWD]-pdk [1]regVal = 0x5, enble = 0x1, inputPipe = 0x2, pipeId = 0x2
[MCU2_1] 41.519489 s: [JWD]layerNum-pdk = 0x1
app_create_graph exiting
app_create_graph done
==========================
Demo : Single Camera w/ 2A
==========================
p: Print performance statistics
s: Save Sensor RAW, VISS Output and H3A output images to File System
e: Export performance statistics
x: Exit
Enter Choice: 11.106000 s: ISS: Starting sensor [IMX390-UB953_D3] ... !!!
==========================
Demo : Single Camera w/ 2A
==========================
p: Print performance statistics
s: Save Sensor RAW, VISS Output and H3A output images to File System
e: Export performance statistics
x: Exit
Enter Choice: [MCU2_1] 41.552978 s: ImageSensor_RemoteServiceHandler: IM_SENSOR_CMD_STREAM_ON
[MCU2_1] 41.553044 s: IM_SENSOR_CMD_STREAM_ON: channel_mask = 0x1
[MCU2_1] 41.553077 s: Starting camera # 0
[MCU2_1] 41.553118 s: Entering IssSensor_Start
[MCU2_1] 41.563564 s: enableUB960Streaming ub960InstanceId = 0
[MCU2_1] 41.563621 s: ub960_cfgScript : ub960I2cAddr = 0x3d
[MCU2_1] 41.563649 s: UB960 config start
[MCU2_1] 41.579624 s: End of UB960 config
[MCU2_1] 41.579690 s: ub960_cfgScript : ub960I2cAddr = 0x3d
[MCU2_1] 41.579722 s: UB960 config start
11.373000 s: ISS: Starting sensor [IMX390-UB953_D3] ... !!!
[MCU2_1] 41.819616 s: End of UB960 config
frm_loop_cnt 0...
frm_loop_cnt 1...
frm_loop_cnt 2...
frm_loop_cnt 3...
frm_loop_cnt 4...
frm_loop_cnt 5...
frm_loop_cnt 6...
frm_loop_cnt 7...
frm_loop_cnt 8...
frm_loop_cnt 9...
frm_loop_cnt 10...
frm_loop_cnt 11...
frm_loop_cnt 12...
frm_loop_cnt 13...
frm_loop_cnt 14...
frm_loop_cnt 15...
frm_loop_cnt 16...
frm_loop_cnt 17...
frm_loop_cnt 18...
frm_loop_cnt 19...
frm_loop_cnt 20...
frm_loop_cnt 21...
frm_loop_cnt 22...
frm_loop_cnt 23...
frm_loop_cnt 24...
frm_loop_cnt 25...
frm_loop_cnt 26...
frm_loop_cnt 27...
frm_loop_cnt 28...
frm_loop_cnt 29...
frm_loop_cnt 30...
frm_loop_cnt 31...
frm_loop_cnt 32...
frm_loop_cnt 33...
frm_loop_cnt 34...
frm_loop_cnt 35...
frm_loop_cnt 36...
frm_loop_cnt 37...
frm_loop_cnt 38...
frm_loop_cnt 39...
J7EVM@QNX#
Please check attached logs and could you let me know how to debug this for eDP display using vision_apps?
Thanks,