Part Number: TDA2EXEVM
Hi,
I have a need to use HDMI local display to show RDM data output of 2D-FFT. I have created a usecase and modified the PkDetect Alg to get a copy of one of the 4 EVEs' 2D-FFT output and create a VideoFrameBuffer to output the RDM data to fftHeatMap for local display. As far as I know the usecase runs without any issue but plugging the HDMI output from the TDA2 cascade board to a monitor showed no HDMI output. It didn't look like there is even sync signal detected by the monitor. Normally when monitor picks up a sync, it has a very gent click to kick the monitor active and show the content. There isn't such a thing on this cascade board.
Was the HDMI connector on the board designed to be used with usecase?
Thanks,
--Khai