Other Parts Discussed in Thread: TMS320TCI6488
Hi,
I have executed 'cfgdemo' example in ndk tools on TMS320TCI6488 EVM.
It displays the following:
/******
TCP/IP Stack Client Configuration Demo
220 bytes required for save
Core Number on which NDK is running = 0
Since EFUSE MAC address is Zero we use the MAC Address = 00-01-02-03-04-05
Only on CORE 0: SGMII reset successful........
Only on CORE 0: SGMII config successful........
Only on CORE 0: SerDes should be up and running
EMAC has been started successfully
Registeration of the EMAC Successful
Service Status: Telnet : Enabled : : 000
Service Status: HTTP : Enabled : : 000
GetIP Ready
EchoSrv Initialized
DataSrv Initialized
NullSrv Initialized
OobSrv Initialized
V6EchoSrv Initialized
Link Status: 100Mb/s Full Duplex on PHY 1
*****/
How to assign a static ip to the EVM. Please help. The NDK user guide is not clear on this.
Regards
Sharath