Part Number: TMS320C6678
Other Parts Discussed in Thread: TXS0108E
Tool/software: Code Composer Studio
Hi,
I used the following codes to set and read the state of 6678's GPIO_12, the version of sdk is: mcsdk_02_01_02_06.
CSL_GpioHandle hGpio;
U8int uiNumber = 12, inData;
hGpio = CSL_GPIO_open (0); // Open the CSL GPIO Module 0
CSL_GPIO_setPinDirInput (hGpio, uiNumber); // Set to INPUT
CSL_GPIO_getInputData(hGpio, uiNumber, &inData);
My problem is when the TXS0108E, a level conversion chip directly connected to GPIO_12, outputs a low level, the low level signal cannot be correctly received by GPIO. I found that the voltage of GPIO was 1.13V. When I use an ammeter to connect the GPIO12 to GND, although the GPIO_12 is set to the input state, It can detect a current of 8mA. Isn't it unreasonable to have so much current in the input state? Or is there something wrong with the configuration codes?
Thanks!