Hi Team,
We are interfacing a new DDR3 part number that is different from the one that is available on the K2G evaluation board.
To configure the DDR3 and to interface it with the 66AK2G12 processor, we are using the following procedure.
1. Use the DDR3 register configuration spreadsheet tool to determine the PHY and CONFIG register values of the DDR3 controller.
2. Populate the new register values in the "\ti\board\src\evmK2G\evmK2G_ddr.c" file and include it as a part of the project.
Can you confirm if this is the expected procedure to configure a new DDR3 part with the processor.
--> NOTE : In the evmK2G_ddr.c file and the register calculation spreadsheet there are few PHY registers that we can't map with each other. Any help would be great in this regard.
And since we are migrating from 24MHz to 25MHz crystal and also with the new DDR3 part number, can the existing MLO file that we have been using be continued as it is. Or do we need to alter the MLO file to support these major changes.?
Also can you share the procedure for editing the .gel file to test these changes through JTAG as well.
Thanks in Advance.
Regards,
Krishna.