Hi,
I'm working on AM572x GP EVM board.The SDK version is ti-processor-sdk-linux-rt-am57xx-evm-06.03.00.106.
I need to Booting U-Boot from the UART.
I have found some resoureces as below:
But I have some error:
antoine@UBUNTU01:~$ picocom -b115200 -d8 -pe -fn -s "sx -kb" /dev/ttyUSB0
picocom v1.7
port is : /dev/ttyUSB0
flowcontrol : none
baudrate is : 115200
parity is : even
databits are : 8
escape is : C-a
local echo is : no
noinit is : no
noreset is : no
nolock is : no
send_cmd is : sx -kb
receive_cmd is : rz -vv
imap is :
omap is :
emap is : crcrlf,delbs,
Terminal ready
*** file: /home/antoine/u-boot-spl.bin
sx -kb /home/antoine/u-boot-spl.bin
Sending /home/antoine/u-boot-spl.bin, 391 blocks: Give your local XMODEM receive command now.
Retry 0: Receiver Cancelled
Transfer incomplete
*** exit status: 128
I found that other people also have the problem:
-https://e2e.ti.com/support/processors/f/791/p/516467/1884780#pi316653=2
About this answer:"Also don't forget to add #define CONFIG_SPL_YMODEM_SUPPORT in beagle_x15.h to include x-modem support in u-boot (this is necessary for UART boot)"
where is this path located in the ti-processor-sdk-linux-rt-am57xx-evm-06.03.00.106?
Any answer will be best wished.
syy
antoine@UBUNTU01:~$ picocom -b115200 -d8 -pe -fn -s "sx -kb" /dev/ttyUSB0
picocom v1.7
port is : /dev/ttyUSB0
flowcontrol : none
baudrate is : 115200
parity is : even
databits are : 8
escape is : C-a
local echo is : no
noinit is : no
noreset is : no
nolock is : no
send_cmd is : sx -kb
receive_cmd is : rz -vv
imap is :
omap is :
emap is : crcrlf,delbs,
Terminal ready
*** file: /home/antoine/u-boot-spl.bin
sx -kb /home/antoine/u-boot-spl.bin
Sending /home/antoine/u-boot-spl.bin, 391 blocks: Give your local XMODEM receive command now.
Retry 0: Receiver Cancelled
Transfer incomplete
*** exit status: 128