Part Number: DRA829VXEVM
Other Parts Discussed in Thread: TCA6408
Hi,
I verified that when AR0820-FPDLINKIII when is connected via the Fusion board, the out-of-the-box application 'single_camera' works and the video is displayed.
Now I'm trying to connect CSI2 camera AR0820 (without FPD-LINKIII module) directly to J52 (CSI2 Expansion Connector) to use native CSI2 interface while using the same driver (I know that all SERDES configuration are in vain). For some reason, the sensor module is stuck in reset.
Can you please point me to the specific location in which this signal is asserted?
Thanks,
Matan