This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-DRA8X-TDA4X: [TDA4] Facing error when call a r5f kernel.

Part Number: PROCESSOR-SDK-DRA8X-TDA4X

Hi,

I have a pre-existing kernel on C66. I want to move it to r5f core. I have included its target libraries also. But when i run the code, it is showing an error of 

0.379000 s: VX_ZONE_ERROR:[ownInitNodeObjDesc:145] ownInitNodeObjDesc: invalid target or no target, associated with kernel

0.379000 s: VX_ZONE_ERROR:[vxCreateNodeByStructure:85] vxCreateNodeByStructure: Failed to create node with kernel enum 0

Could you please help me with this.

Regards,

Hruday