Part Number: TMS320C6678
Hello Champs,
Customer combined helloWorld and IPC project, please see below snapshots.
The IPC, clock, DDR, ethernet initialization are all passed in main(). Then entering in tsk0.
a. Core0: initializing NDK, creating UDP transmit task(priority is 5, the other tasks' priority is 1), if UDP doesn't get Tx flag, then Tasksleep->TestTask1;
b. Core1: task_yeild->TestTask1.
TestTask1: synchronizing core0 and core1. It will prompt error message when entering Notify() in core0. Please see below error.