This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VMXEVM: Build PDK example; generate .out file

Part Number: TDA4VMXEVM

Hi,

I've followed the steps on SDK RTOS user guide to load and run a PDK example in J721E EVM using CCS.

In order to build a DSS example, I used the following command: 

make -s dss_display_testapp BOARD=j721e_evm CORE=mcu2_1 BUILD_PROFILE=debug

After the building is done, I only can see the following file in  PDK_INSTALL_DIR/packages/ti/binary/dss_display_testapp/bin/j721e_evm

Normally, a .out file is supposed to be generated, am I right?

Please let me know how I can generate the executable file that I need to load in CCS to the EVM.

Thanks,

Brahim