Hi,
The question is about TCI6638K2K:
Is it possible for the ALE of the 10GBe to filter incoming multicast frames in VLAN unaware mode?
SPRUHJ5 documentation page 68 (2-42) states in the ALE rules:
If (VLAN_Unaware)
FORCE_UNTAGGED_EGRESS = “000000”
REG_MCAST_FLOOD_MASK = “111111”
UNREG_MCAST_FLOOD_MASK = “111111”
VLAN_MEMBER_LIST = “111111”
So this will flood all mcast frames to all ports.
How can we receive ONLY desired mcast frames with destination addresses that we enter in the ALE Table in VLAN unaware mode?
Or is it better to move to VLAN Aware mode but how can we keep the VLAN part transparent when we do not have VLAN tags in the frames?
Best Regards,
Marius