Hello,
on the ARM side of the OMAP-L137 I upgraded the SYS/BIOS to Version: 6.30.03.46
The new SYS/BIOS has for the module ti.sysbios.timers.timer64.Timer new fields (compared with my older DSP/BIOS):
- ownerCoreID with a default value of 0.
Where can I find documentation about the mapping of this "0" to ARM/DSP?
Or in other words: With this default value of 0 is the ARM or the DSP the owner?
- intFreqs[2]
The Arm is only using upper half of timer1.
Has the setting of intFreqs[0].lo by the ARM any influence to timer0 (which is used only by the DSP)?
Used CCS Version : 4.2.1.00004
Thanks,
Frank