Tool/software: Code Composer Studio
Hi,
I have a problem starting debug session from CCS 5.5 (CGT 7.4.23), emulator XDS100v1 attached to a C6678 EVM.
From a workspace and project that debug without problem since few days ago, when I try to launch the debugger a get the message:
Cannot read System Setup data from XML file cvm.ccxml
boost:filesystem:status: directory of file damaged and not readable:
"C:\User\.username\AppData\Local\.TI\226004662\0\0\226941379.cache"
The environment was not changed from the privous sucessfull debug session.
I tried with other workspace/project with the same results. I tried with create another Target configuration file but the result does not change.
I recently install CCS 10, but I'm quite sure the CCS5 5.5 debugger still working after the installation.
There is way to fix the problem? Maybe can I delete the cache files?