Part Number: TMDSIDK437X
Hi
I am adding Ethernet IP capability to my project and have started with the idk am437x ethernet ip example project : ethernetip_adapter_am437x_arm
I was able to perform project create proccess , successful compile the code and connect via uart.
at boot , the firmware UART indicates that it is using IP 255.255.255.255
I connect the laptop to the am437x IDK and get one green led and one flashing green led
When I try to use the EIP tool and enter this address in the "station" text box , I am unable to find the device.
can you help me get this demo running
1) can I get the binaries - to help make sure no issue woth compilation\PDK etc ?
2) is there a special configurations I should do on the PC side ? what should I see when I run IPCONFIG ?
3) Do I need to edit subnext mask ? if so , how to I do that : while the UART interface seems to supports changing the ip address, I could not find how do I change the subnet mask
4) I have experience with the TI Ethercat demo that allows toggling LEDs via Twincat. is there a similar demo with Ethernet IP ? i
Thanks
R2