Other Parts Discussed in Thread: OMAP-L138, OMAPL138
http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/t/56589.aspx
http://e2e.ti.com/support/embedded/f/353/p/86333/298058.aspx
So i've been trying to find a solution to a problem that may or may not exist, idk i have a lot of time on my hands so i'm trying to get armubl-03.20.00.14 working with my logic pd evm kit for omap l138.
between the two of these forums i've gotten things mostly working
when i boot my device i get an error
FMD:ReadID Device not Supported Mfg=0x0, Dev=0x0 0x0 0x0
ERROR: EBOOT: FMD_Init call failed!
ERROR: Invalid device info found! fourcing default values
so I'm assuming that because i didn't change the device type i'm getting this error, I don't know how to change the device type to match my boot rom image, was he talking about the wince side or the in the armubl source or is this a whole new and improved problem?
If there is a guide to do this i couldn't find it, at least one that had a enough details with my particular verion