Can someone tell me (or point me to a document) what the latency of the H.264 encoder is? I understand that there is algorithm latency (e.g. the algorithm takes 14.4 ms until it spits out an answer), but is there multiframe latency associated with the encoder? Does the encoder need multiple frames buffered before it can produce an initial frame?
My application has an airborne platform taking imagery and broadcasting it to the ground over IP. The transport stream is TBD. We currently are broadcasting NTSC over a video link, but now would like to move this to an IP radio with a transport stream. Therefore overall latency is important, hence the question on the encoding latency internal to the DaVinci.
I'm using the DM6467 at 729 MHz and would be setting up the encoder with IVIDEO_LOW_DELAY.