This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2EG-17: DCAN triple-sampling not supported

Part Number: TDA2EG-17

Hi

My SDK version is processor-sdk-linux-automatic 6_ 00_ 00_ 03。

When I want to set DCan to triple sampling mode, why do the following errors occur

root@hi-target:/mnt/firmware# ip link set can0 type can bitrate 50000 triple-sampling on
RTNETLINK answers: Operation not supported

The test found that only two modes of triple sampling and one-shot will report this error, and other modes can be set normally


[ loopback { on | off } ]
[ listen-only { on | off } ]
[ triple-sampling { on | off } ]
[ one-shot { on | off } ]
[ berr-reporting { on | off } ]