I have a question about UART of AM3352. With the stop bit set to 2 bits in UART,When receiving data, if the stop bit is 2bit data, is the UART ready to recognize the start bit of the next data after recognizing the first stop bit? The AM3352 datasheet states that it is 16C750 compatible. The 16c750 data sheet contains ``(SHT27) The receiver clocks only the first stop bit, regardless of the number of stop bits selected.The number of stop bits generated, in relation to word length and bit 2, is shown in Table 7. "It has been described as.