Part Number: AMIC110
Other Parts Discussed in Thread: TMDXICE110
Hi,
we designed a custom board with the AMIC110 pretty much similar to the Evaluation Board TMDXICE110 (circuit shematics appended). However, on all prototypes we encouter the same problem while running one of the Ethercat sample applications. If Twincat is connected to the board via PHY1 (phy addr 1 / D700 in circuit shematics) everything is working as expected. However, if we connect the cable via the other PHY2 (D800 in circuit shematics / adddr 13) it is not working.
Investigations with the oscilloscope on the phy2 signals showed, that while Ethercat packages are sent from Twincat (also visble with WireShark) the PHY is sending data on the RX[0:3] lines (most likely reception OK, also no RX_error). The phy clocks show good signal as well. However, no signals on the TX lines as well as no TX_EN signal. In the Software Initialisation both PHYs are found on the MDIO bus with its correct addresses and the registers can be read and written to. So far we are not able to narrow to problem to either a Software or Hardware Problem and any input is highly appreciated.
Thank you very much in advance and best regards
Philipp
/cfs-file/__key/communityserver-discussions-components-files/791/amic110_5F00_problem.zip