Other Parts Discussed in Thread: DM3730, OMAP3530
Hi,
We are trying to migrate from the OMAP3530 to DM3730. The OMAP3530 currently being used in our product uses POP (Package-on-Package) for LPDDR. But, for the DM3730 we would like to not do that (not use POP) and put the LPDDR on the PCB itself. However, it shows on the datasheet for the DM3730 that the only package that would let us do that is the CUS package with 423-pins. The POP packages (CBP and CBC) have 515 pins.
The question is:
- if we are migrating from an OMAP3530 which uses POP for LPDDR to a DM3730 which would use non-POP LPDDR, is everything else going to stay the same? Or due to less number of pins, pin-muxing is extensive on the CUS package and we would have to do major software changes for other interfaces?
- How different are the pin-muxing on the different packages of the DM3730?
- Why are there way more pins on the CBP and CBC packages (NC pins?)?
Your help is much appreciated.
-Mahdi